Maybe I’m not so close as I thought. I use Eagle 4.14; I set the minimum clearance to 10 mil and passed the Eagle DRC, but then I failed the online DRC. The message was:
Checked Aperture 11 (8,0.0520): Failed
Error - Aperture too thin
How do I find the offending point on the board?
[OT] How do I attach a file here?
Jake
i promise i will fix this bug ASAP!
Ok whats happening is that Eagle uses octagonal pads which are made using a Macro which accepts a parameter.
At the moment i have not yet handled macro’s, BUT i promise i will do it ASAP. For the moment i will just ignore them (ie not check them) but i will be able to give a warning (not an error) when a macro’s parameter fails just might take a while to get that working.