Hey all,
I’m new to Eagle so please excuse me. I’ve added a 74HC595 shift register to my schematic and at first, I couldn’t find the VCC and GND connections for it. Then, I used Eagle’s invoke command to get them to appear below them. But now, am in a fix, I want the shift register to be powered by +5V and not VCC because it is something like 9V and such a high voltage will fry the IC for sure.
Schematic:
http://i42.tinypic.com/2i8x0k6.png
I’m using a 7805A to get regulated +5V. Now, however, when I switch to the board layout, I see that the VCC of shift register is connected to the battery input which is clearly NOT what I intend. As shown:
http://i44.tinypic.com/261jamb.png
I’m using Eagle 6. What do I do to get it to connect to +5V instead of VCC?