7402 Library Power Question

So I want to work on building a 2 to 4 line decoder using just 74AC04 and a 74AC08 but I cannot find the VCC and VDD pins in Eagle Cad. Can someone point me in the right direction?

They are present but they aren’t shown to avoid clutter.

IMO not showing the supply pins is an obsolete method of drawing schematics.

All connected pins should be shown, a reader of the schematic may not be aware of the pinout of the IC or which are the power pins.

I suppose that they are automatically connected to VCC/GND nets too?

What if he designer uses different names for those nets? = no connection.

You can use the “invoke” tool/command to display the power pins.

It looks like an eye.

never mind. I found it, I just needed to use the vcc supply pins instead of the 5v supply pin.

Thanks everyone!