I am trying to make a board using the PIC18F13K50 in SSOP format but am having trouble getting a eagle part.
I have made a prototype circuit using a PIC18F4550 on a breadboard and now I want to make the real thing on a board but I dont’ want to use up the chip I use for experimenting. I already have a few PIC18F13k50’s and would like to use one of them instead, but I am having a ton of trouble making my own part in eagle. I have even tried editing a similar part that was the same size/format/number of pins and had trouble doing that too.
Does anyone happen to have the PIC18F13K50 eagle part on hand? Or does anyone know if it’s possible to add a “blank” 20 pin SSOP part where I could just it and it’s leads (not worrying about electrical connections or whatnot?).
I am building a solar hot water pump controller that uses two temp sensors to only turn the pump on when the panel is warmer then the water in my storage tank by a certain amount.