Eagle pin swappability in the library parts

hello,

i cannot find specific instructions about Eagle for putting a dual LTC1841 comparator in the library and enabling pin swapping…i have done it in the schematic but i am sure this is wrong…i made a symbol for comparator_a, another symbol for comparator_b, another symbol for V+_V- (power).

i then put them together in a device with the footprint making sure that the above symbols had equivalent names to those on the footprint…but this just doesn’t seem right.

i wish to pin swap in cse in the layout , one of the comparators is in a better position (i will only be using one of them)

-its the bit about naming the pins on the various symbols that confuses me.

-also, to get pin swappability, is it really just as easy as changing “swap level” to “1” for all those pins i wish to swap…presumably invertin ginputs and noninverting inputs cannot have the same swap level number, as they are obviously not swappable?

I believe that when you make the device, you change the swap level for the symbols, not for the pins. I haven’t made any parts with ‘internal’ parts that can be swapped, so I’m not sure.

Stig