Just got an easyWEB 3 board and I’m wondering if it has a problem…
Out of the box I connect the board to my network through a network switch, configure my desktop computer on the 192.168.0.x network(easyweb defaults to 192.168.0.30), and try to connect via web browser to the board.
I often have to make multiple attempts to connect to the board before it actually generates a web page …and sometimes it actually generates a complete web page. Most of the time the page that is generated is incomplete (doesn’t show the ADC graphs and the web browser is left spinning its wheels) and most often when the page auto refreshes the transaction hangs. I’ve tried Mozilla, IE and Konquerer browsers.
Is this normal behavior for the easyweb board and demo software, or is there a problem with the board?