EM-406 GPS troubles

I have a max232 setup on a bread board with an atmega8 chip, i have got it to work fine and do various things like turn on LEDs and manipulate data i send to it through the com port etc so i know it works fine.

I connected my EM-406 module to my max232 chip, and this is what it spits out.

4GPRMs.0???5³.0³6/V,291??7,*2Ìóá<GPwGq.8???57.0³6/,0/0?/,M,0/0/M,0???«5³

4GPwSA.q.1/,*1Ñóa³4M­ÚsöööVvç†6göf

Sorry, i have worked it out.

My microcontroller was still connected and it was editing the information.

All working good, just time to get it close to a window for a fix.