Hello every one !
I recently bought a GPS EM-406A.
I directly plug the GPS to my PIC and it’s working but with some troubles.
When I open the EM-406A datasheet, I can see : RS232 level.
My question : Do I need a MAX 232 or something like that to inerface the GPS to my 18f4520 ?
Best regards
Hoffmann
PS : It is also written :
TTL level, Output voltage level: 0V ~ 2.85V