Hi,
I bought an EM406A module a couple of weeks ago. I connected it to the serial port of my PC through a level converter(2.85 to 5v) and a MAX 232 circuit.
I configured the hyperterminal of the PC to work at 4800 baud rate, and 8 bits and one stop bit, no parity.
However,the GPS module is not locking at all. The LED does light up continually. But I’m getting the output in the following manner:
$GPGGA,164310.088,0,00,M,0.0,M,0000*57
$GPGSA,A,1,*1E
$GPRMC,164310.088,V,060710,*2E
I’ve kept the receiver on for quite some time now (around 30mins) but still the GPS doesn’t lock.
What could be the problem here?
Is there some problem with my connections?