Anyone have an EM-408 running?
Is the default data output NMEA 0183 at 4800?
The data sheet says that the rate is variable and doesn’t specify if NMEA or Sirf is default . What I see doesn’t look line NMEA at 4800. I haven’t tried anything too technical yet, but on the Tx pin all I get is a constant 0.75V, with no gaps (0V) to indicate spaces between messages…
-
Think I need to send a Sirf message to change to NMEA?
-
Is so, anyonw know what the default data setting are for globalsat’s Sirf?
Also, what does everyone do with the Enable pin?
The usglobalsat datasheet just specifies that this in on/off, and the globalsat.tw datasheet shows no connection (NC).
All help is greatly appreciated!!! Until now I’ve had my project hooked to a garmin, outputing NMEA at 4800 and it works fine. I hooked up the EM408 and am getting nothin’…
Thanks