Error loading adc_lpmode0_dma Ambiq SDK example onto redboard Artemis ATP

To whom it may concern,

I tried to modify the adc_lpmode0_dma example Makefile to upload this example from C code to the red board Artemis ATP. I added the board_sfe, with the SparkFun board definitions, directory to the SDK following a Sparkfun tutorial. I put the modified Makefile in the original directory of the adc_lpmode0_dma example provided by the Ambiq SDK in the Apollo3_evb directory.

I attached a copy of my make file to this post. When I try to load this example to the board I get the following output from the make:

"Compiling gcc ../src/adc_lpmode0_dma.c

Compiling gcc ../../../../../utils/am_util_delay.c

Compiling gcc ../../../../../utils/am_util_faultisr.c

Compiling gcc ../../../../../utils/am_util_stdio.c

Compiling gcc ../../../../../devices/am_devices_led.c

Compiling gcc startup_gcc.c

Linking gcc bin/adc_lpmode0_dma_svl.axf with script /Users/miayanyeremi/Downloads/AmbiqSuite-R2.4.2/boards_sfe/common/tools_sfe/templates/asb_svl_linker.ld

/usr/local/gcc_arm/gcc-arm-none-eabi-9-2020-q2-update/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld: bin/adc_lpmode0_dma_svl.axf section .stack' will not fit in region sram’

/usr/local/gcc_arm/gcc-arm-none-eabi-9-2020-q2-update/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld: region `sram’ overflowed by 4088 bytes"

I don’t know what to do to try and fix this error I didn’t modify the original c code. Any help or suggestions would be appreciated.

Cheers,

Miayan

I could not get my make file to attach to this post so here it is copy and pasted:

TARGET := adc_lpmode0_dma

COMPILERNAME := gcc

PROJECT := adc_lpmode0_dma_gcc

CONFIG := bin

SHELL:=/bin/bash

Setup

TOOLCHAIN ?= arm-none-eabi

PART = apollo3

CPU = cortex-m4

FPU = fpv4-sp-d16

Default to FPU hardware calling convention. However, some customers and/or

applications may need the software calling convention.

#FABI = softfp

FABI = hard

LINKER_FILE := ./adc_lpmode0_dma.ld

STARTUP_FILE := ./startup_$(COMPILERNAME).c

Required Executables

CC = $(TOOLCHAIN)-gcc

GCC = $(TOOLCHAIN)-gcc

CPP = $(TOOLCHAIN)-cpp

LD = $(TOOLCHAIN)-ld

CP = $(TOOLCHAIN)-objcopy

OD = $(TOOLCHAIN)-objdump

RD = $(TOOLCHAIN)-readelf

AR = $(TOOLCHAIN)-ar

SIZE = $(TOOLCHAIN)-size

RM = $(shell which rm 2>/dev/null)

EXECUTABLES = CC LD CP OD AR RD SIZE GCC

K := $(foreach exec,$(EXECUTABLES),\

$(if $(shell which $($(exec)) 2>/dev/null),\

$(info $(exec) not found on PATH ($($(exec))).)$(exec)))

$(if $(strip $(value K)),$(info Required Program(s) $(strip $(value K)) not found))

ifneq ($(strip $(value K)),)

all clean:

$(info Tools $(TOOLCHAIN)-$(COMPILERNAME) not installed.)

$(RM) -rf bin

else

DEFINES = -DPART_$(PART)

DEFINES+= -DAM_PACKAGE_BGA

DEFINES+= -DAM_PART_APOLLO3

DEFINES+= -Dgcc

SDKPATH = /Users/miayanyeremi/Downloads

BOARDPATH = $(SDKPATH)/AmbiqSuite-R2.4.2/boards_sfe/redboard_artemis_atp

#INCLUDES = -I../../../bsp #CHANGED

INCLUDES+= -I$(BOARDPATH)/bsp

INCLUDES+= -I../src

INCLUDES+= -I../../../../../mcu/apollo3

INCLUDES+= -I../../../../../CMSIS/AmbiqMicro/Include

INCLUDES+= -I../../../../../devices

INCLUDES+= -I../../../../..

INCLUDES+= -I../../../../../utils

INCLUDES+= -I../../../../../CMSIS/ARM/Include

VPATH = ../src

VPATH+=:../../../../../utils

VPATH+=:../../../../../devices

SRC = adc_lpmode0_dma.c

SRC += am_util_delay.c

SRC += am_util_faultisr.c

SRC += am_util_stdio.c

SRC += am_devices_led.c

SRC += startup_gcc.c

CSRC = $(filter %.c,$(SRC))

ASRC = $(filter %.s,$(SRC))

OBJS = $(CSRC:%.c=$(CONFIG)/%.o)

OBJS+= $(ASRC:%.s=$(CONFIG)/%.o)

DEPS = $(CSRC:%.c=$(CONFIG)/%.d)

DEPS+= $(ASRC:%.s=$(CONFIG)/%.d)

#LIBS = ../../../bsp/gcc/bin/libam_bsp.a #CHANGED

LIBS = $(BOARDPATH)/bsp/gcc/bin/libam_bsp.a

LIBS += ../../../../../mcu/apollo3/hal/gcc/bin/libam_hal.a

CFLAGS = -mthumb -mcpu=$(CPU) -mfpu=$(FPU) -mfloat-abi=$(FABI)

CFLAGS+= -ffunction-sections -fdata-sections -fomit-frame-pointer

CFLAGS+= -MMD -MP -std=c99 -Wall -g

CFLAGS+= -O0

CFLAGS+= $(DEFINES)

CFLAGS+= $(INCLUDES)

CFLAGS+=

LFLAGS = -mthumb -mcpu=$(CPU) -mfpu=$(FPU) -mfloat-abi=$(FABI)

LFLAGS+= -nostartfiles -static

LFLAGS+= -Wl,–gc-sections,–entry,Reset_Handler,-Map,$(CONFIG)/$(TARGET).map

LFLAGS+= -Wl,–start-group -lm -lc -lgcc $(LIBS) -Wl,–end-group

LFLAGS+=

Additional user specified CFLAGS

CFLAGS+=$(EXTRA_CFLAGS)

CPFLAGS = -Obinary

ODFLAGS = -S

COMMONPATH = $(SDKPATH)/AmbiqSuite-R2.4.2/boards_sfe/common

Bootloader Tools

AMBIQ_BIN2BOARD=$(PYTHON3) $(COMMONPATH)/tools_sfe/ambiq/ambiq_bin2board.py

ARTEMIS_SVL=$(PYTHON3) $(COMMONPATH)/tools_sfe/artemis/artemis_svl.py

Rules

#all: directories $(CONFIG)/$(TARGET).bin

all: asb

asb: directories $(CONFIG)/$(TARGET)_asb.bin

svl: directories $(CONFIG)/$(TARGET)_svl.bin

directories: $(CONFIG)

$(CONFIG):

@mkdir -p $@

$(CONFIG)/%.o: %.c $(CONFIG)/%.d

@echo " Compiling $(COMPILERNAME) $<" ;\

$(CC) -c $(CFLAGS) $< -o $@

$(CONFIG)/%.o: %.s $(CONFIG)/%.d

@echo " Assembling $(COMPILERNAME) $<" ;\

$(CC) -c $(CFLAGS) $< -o $@

$(CONFIG)/$(TARGET)_asb.axf: LINKER_FILE = $(COMMONPATH)/tools_sfe/templates/asb_linker.ld

$(CONFIG)/$(TARGET)_asb.axf: $(OBJS) $(LIBS)

@echo " Linking $(COMPILERNAME) $@ with script $(LINKER_FILE)";\

$(CC) -Wl,-T,$(LINKER_FILE) -o $@ $(OBJS) $(LFLAGS)

$(CONFIG)/$(TARGET)_svl.axf: LINKER_FILE = $(COMMONPATH)/tools_sfe/templates/asb_svl_linker.ld

$(CONFIG)/$(TARGET)_svl.axf: $(OBJS) $(LIBS)

@echo " Linking $(COMPILERNAME) $@ with script $(LINKER_FILE)";\

$(CC) -Wl,-T,$(LINKER_FILE) -o $@ $(OBJS) $(LFLAGS)

$(CONFIG)/$(TARGET)%.bin: $(CONFIG)/$(TARGET)%.axf

@echo " Copying $(COMPILERNAME) $@…" ;\

$(CP) $(CPFLAGS) $< $@ ;\

$(OD) $(ODFLAGS) $< > $(CONFIG)/$(TARGET).lst

#$(CONFIG)/$(TARGET).axf: $(OBJS) $(LIBS)

@echo " Linking $(COMPILERNAME) $@" ;\

$(CC) -Wl,-T,$(LINKER_FILE) -o $@ $(OBJS) $(LFLAGS)

#$(CONFIG)/$(TARGET).bin: $(CONFIG)/$(TARGET).axf

@echo " Copying $(COMPILERNAME) $@…" ;\

$(CP) $(CPFLAGS) $< $@ ;\

$(OD) $(ODFLAGS) $< > $(CONFIG)/$(TARGET).lst

ASB_UPLOAD_BAUD = 115200

SVL_UPLOAD_BAUD = 921600

COM_PORT = /dev/cu.wchusbserial1410

bootload_asb: directories $(CONFIG)/$(TARGET)_asb.bin

$(AMBIQ_BIN2BOARD) --bin $(CONFIG)/$(TARGET)_asb.bin --load-address-blob 0x20000 --magic-num 0xCB -o $(CONFIG)/$(TARGET) --version 0x0 --load-address-wired 0xC000 -i 6 --options 0x1 -b $(ASB_UPLOAD_BAUD) -port $(COM_PORT) -r 2 -v

bootload_svl: directories $(CONFIG)/$(TARGET)_svl.bin

$(ARTEMIS_SVL) $(COM_PORT) -f $(CONFIG)/$(TARGET)_svl.bin -b $(SVL_UPLOAD_BAUD) -v

bootload: bootload_svl

clean:

@echo “Cleaning…” ;\

$(RM) -f $(OBJS) $(DEPS) \

$(CONFIG)/$(TARGET)%.bin $(CONFIG)/$(TARGET)%.axf \

$(CONFIG)/$(TARGET).lst $(CONFIG)/$(TARGET).map

$(RM) -r bin

-$(RM) $(TARGET).ld

$(CONFIG)/%.d: ;

#../../../bsp/gcc/bin/libam_bsp.a:

$(MAKE) -C ../../../bsp

#../../../../../mcu/apollo3/hal/gcc/bin/libam_hal.a:

$(MAKE) -C ../../../../../mcu/apollo3/hal

Automatically include any generated dependencies

#-include $(DEPS)

#endif

#.PHONY: all clean directories

$(SDKPATH)/mcu/apollo3/hal/gcc/bin/libam_hal.a:

$(MAKE) -C $(SDKPATH)/mcu/apollo3/hal/gcc

$(SDKPATH)/third_party/uecc/gcc/bin/lib_uecc.a:

$(MAKE) -C $(SDKPATH)/third_party/uecc

$(BOARDPATH)/bsp/gcc/bin/libam_bsp.a:

$(MAKE) -C $(BOARDPATH)/bsp/gcc

Automatically include any generated dependencies

-include $(DEPS)

endif

.PHONY: all clean directories bootload bootload_asb bootload_svl

That appears to be a linker error. The SVL linker takes an additional amount of space (reserved for the SVL bootloader application). I would recommend using the original linker script from the example instead of the modified version. In the SparkFun examples this can be done by specifying the ‘asb’ target. Aka ‘make BOARD=redboard_artemis_atp asb’

When you use the asb linker script you will need to upload using the Ambiq Secure Bootloader (ASB) rather than the SparkFun Variable Loader (SVL)