ESP32-C6 plus drops com port on reset and takes 18 seconds to recover

I have tried to use the C6 for a project using Arduino IDE. My code uploads fine but when I hit the reset button to get the code running, the C6 drops the com port x 18 seconds but starts executing the code immediately. By the time the C6 re-establishes the COM port so I can see what is going on via the serial window in Arduino, the code is down deep into the loop(). I am not able to see anything in the setup() due to the time lag. I have turned in this issue to tech support last week but never recievied any response. Due to time constraints, I had to pull the C6 out of the project pending resolution of this problem. Has anyone else had this issue with the C6 and if so, what was the fix? I do have CDC on boot enabled.

See other thread :slight_smile: