Hi,
I’ve found an issue and a possible solution for this:
I have a Micromod Single Board with an ESP32 plus a Haptic Driver DA7280 connected via Qwiic.
Following the hookup guide and uploading the unaltered I2C example, I get this compile error (compiler exits):
Arduino\libraries\SparkFun_Qwiic_Haptic_Driver_DA7280_Library\src\Haptic_Driver.cpp: In member function 'float Haptic_Driver::getBemf()':
Arduino\libraries\SparkFun_Qwiic_Haptic_Driver_DA7280_Library\src\Haptic_Driver.cpp:502:1: error: control reaches end of non-void function [-Werror=return-type]
502 | }
| ^
cc1plus.exe: some warnings being treated as errors
exit status 1
I was able to workaround this by adding to Haptic_Driver.cpp
Line 501
default:
return 0.0;
Example works then.
I am not sure though if that is the proper solution. Could anyone confirm that or suggest another solution?
I will open a ticket in the Git repo and link this post there.