Good morning,
i bought 2 of these boards and i am trying to upload some code.
I want to use them without Arduino.
https://www.sparkfun.com/products/13287
I am using Arduino IDE 1.8.5 and the usb-ttl converter in pics attached, found it on Amazon:
https://www.amazon.it/gp/product/B01MR7 … UTF8&psc=1
I followed the hookup guide:
https://learn.sparkfun.com/tutorials/es … he-esp8266
I already downloaded and installed the board package and selected “Sparkfun ESP8266 Thing” 115200 baud rate.
Shield switch set on HW.
I connected pins like this:
shield GPIO0 to usb-ttl GND
shield GND to usb-ttl GND
shield 5V to usb-ttl 5V
shield RX to usb-ttl TX
shield TX to usb-ttl RX
The problem is:
"Arduino:1.8.5 (Windows 8.1), Board:“SparkFun ESP8266 Thing, 80 MHz, Flash, Disabled, 512K (no SPIFFS), v2 Lower Memory, Disabled, None, Only Sketch, 115200”
Lo sketch usa 281080 byte (56%) dello spazio disponibile per i programmi. Il massimo è 499696 byte.
Le variabili globali usano 28008 byte (34%) di memoria dinamica, lasciando altri 53912 byte liberi per le variabili locali. Il massimo è 81920 byte.
warning: espcomm_sync failed
error: espcomm_open failed
error: espcomm_upload_mem failed
error: espcomm_upload_mem failed"
These are the steps i performed in order:
-rebooting IDE and circuitry
-disconnecting and reconnecting pins in different orders
-GPIO0 to GND, reboot, keeping it to GND
-GPIO0 to GND, reboot, disconnecting it
-RST and GPIO0 to GND, reboot, keeping them to GND
-RST and GPIO0 to GND, reboot, disconnecting them
-setting shield on SW and retried as up
-using HW TX/RX pins and SW TX/RX pins and retried as up
-changing board with “Generic ESP8266 Wifi module” and retried as up
i am running out of ideas.
Am i doing something wrong? What can i do more?
Thanks,
Nicola