Hi guys,
I am having a bit of trouble in setting up the hardware for my ESP8266 with my UNO. Can anyone point me to the right direction please?
I have read the hook up guide but i think im missing something.
On the ESP8266 WIFI Shield, there is a ESP8266 PROG little section which has the GND, 5V, RX, TX and DTR pin. I have supplied 5v and ground from UNO to 5v and GND pins respectively. I also connected the TX and RX OF esp8266 to UNO RX and TX repectively.
After that I powered it up and try to load up the ESP8266 Wifi Shield Demo example but it is failing to connect to the ESP8266. Have I done something wrong in hooking it up?