Hi,
I’ve seen this topic before, but no answers. I’m hoping that including the code that I’m using will generate a bit more attention.
I’ve been struggling with getting an ANT connection setup with the nRF24AP1 board and USB ANT stick. Sparkfun provides some C code for an ATMega 168, but it appears to have some errors in it. I have worked a lot on this code, and think I have come up with a working solution, but I can’t seem to get the connection established.
http://www.sparkfun.com/products/8840
http://www.sparkfun.com/products/8565
I send 6 packets to the nRF24AP1 board, and confirm that RTS goes high after each packet (confirming proper baud rate, message format, etc.). I have installed the FTDI drivers, and the ANT stick shows up as a COM port. I have a COM sniffer setup for 4800bps, but it shows nothing when I send data. Nor does the LED on the ANT stick light up.
I’ve put a ton of time into this, and am totally lost at this point since I don’t know of any way to diagnose what the problem is. Does anybody have experience with setting up a simple ANT connection, and could take a look at my code? I believe I have commented it adequately.
As a quick reference, I have set the following parameters on my nRF24AP1 module:
network # = 0
channel # = 0
Device # = x0031
Device type ID = x01
channel type = x10
transmission type = x01
Thanks for the help!!
DC
/* 
 * AP1_master.c 
 * 
 * Created: 5/15/2011 4:09:22 PM 
 *  Author: DC 
 */ 
/* 
    07-07-08 
    Copyright Spark Fun Electronics© 2008 
    Aaron Weiss 
   aaron at sparkfun.com 
    
    Master AP1 Intitialization @ 4800bps 
*/ 
#include <stdlib.h> 
#include <stdio.h> 
#include <avr/io.h> 
#include <avr/pgmspace.h> 
//#define FOSC 8000000 // 8MHz         //ORIGINAL 
#define F_CPU 8000000 // 8MHz         //I added 
#define BAUD 4800 
#define MYUBRR 103 // Calculated from http://www.wormfood.net/avrbaudcalc.php 
#define sbi(var, mask)   ((var) |= (uint8_t)(1 << mask)) 
#define cbi(var, mask)   ((var) &= (uint8_t)~(1 << mask)) 
#define STATUS_LED 5 // Pin 28 (PC5) 
// Define functions 
//======================= 
void ioinit(void);      // initializes IO 
static int uart_putchar(char c, FILE *stream); // sends char out of UART 
uint8_t uart_getchar(void); // receives char from UART 
static FILE mystdout = FDEV_SETUP_STREAM(uart_putchar, NULL, _FDEV_SETUP_WRITE); 
void delay_ms(uint16_t x); // general purpose delay 
void config(void); // runs config functions 
//======================= 
// Configuration functions 
//======================= 
void reset(void); 
void assignch(void); 
void setchid(void); 
void opench(void); 
void setchperiod(void); 
void send(void); 
//======================= 
int main (void) 
{ 
    ioinit(); 
    
   sbi(PORTC, STATUS_LED);  //Just to inform that everything is powered up 
    
   config(); 
    
   while(1) 
    { 
    
   sbi(PORTC, STATUS_LED); 
   delay_ms(500); //was 500 
   cbi(PORTC, STATUS_LED); 
   delay_ms(500);  //was 500 
   } 
    return(0); 
} 
void config (void) 
{ 
   reset(); 
   delay_ms(1000);  
   assignch(); 
   delay_ms(1000);  
   setchid(); 
   delay_ms(1000); 
   setchperiod();    
   delay_ms(1000); 
   opench(); 
   delay_ms(1000);  
   send(); 
} 
// Resets module 
void reset (void) 
{ 
   uint8_t i; 
   uint8_t setup[7]; 
    
   //start test code 
   //uint8_t test; 
   //test = 0xA; 
   //putchar('U'); 
   //putchar('A'); 
   //end test code 
    
    
   setup[0] = 0xa4; // SYNC Byte 
   setup[1] = 0x01; // LENGTH Byte 
   setup[2] = 0x4a; // ID Byte 
   setup[3] = 0x00; // Data Byte N (N=LENGTH) 
   setup[4] = 0xef; // Checksum 
   setup[5] = 0x00; // zero pad 
   setup[6] = 0x00; // zero pad 
    
   for(i = 0 ; i < 7 ; i++) 
    { 
   putchar(setup[i]); 
    } 
} 
// Assigns CH=0, CH Type=10(TX), Net#=0 
void assignch (void) 
{ 
   uint8_t i; 
   uint8_t setup[9]; 
    
   setup[0] = 0xa4;   //Sync 
   setup[1] = 0x03;   //Length = 3 bytes 
   setup[2] = 0x42;   //Message ID = assign channel 
   setup[3] = 0x00;   //ch # 0 
   setup[4] = 0x10;   //ch type=10 
   setup[5] = 0x00;   //Network # = 0 
   setup[6] = 0xf5;   //Checksum 
   setup[7] = 0x00;   // zero pad 
   setup[8] = 0x00;   // zero pad 
   for(i = 0 ; i < 9 ; i++) 
    { 
   putchar(setup[i]); 
    } 
} 
// Assigns Device#=3100 (actually 31 - little endian), Device Type ID=01, Trans Type=01 
void setchid (void) 
{ 
   uint8_t i; 
   uint8_t setup[11]; 
    
   setup[0] = 0xa4;   //Sync byte 
   setup[1] = 0x05;   //Length = 5 bytes 
   setup[2] = 0x51;   //message ID = set channel ID 
   setup[3] = 0x00;   //ch # 0 
   setup[4] = 0x31;   //Device number = 0031 (little endian), so 31 here 
   setup[5] = 0x00;   //Device number = 0031 (little endian), so 00 here 
   setup[6] = 0x01;   //Device type ID = 01 
   setup[7] = 0x01;    //WAS 0x05.  This is transmission type, and I changed to 0x01 (no shared address) as in example on p16 of ANT guide 
   setup[8] = 0xc1;   //checksum 
   setup[9] = 0x00; // zero pad 
   setup[10] = 0x00; // zero pad 
    
   for(i = 0 ; i < 11 ; i++) 
    { 
   putchar(setup[i]); 
    } 
} 
// Opens CH 0 
void opench (void) 
{ 
   uint8_t i; 
   uint8_t setup[7]; 
    
   setup[0] = 0xa4;   //sync 
   setup[1] = 0x01;   //length = 1 
   setup[2] = 0x4b;   //message ID = open channel 
   setup[3] = 0x00;   //ch # 0 
   setup[4] = 0xee;   //checksum 
   setup[5] = 0x00; // zero pad 
   setup[6] = 0x00; // zero pad 
    
   for(i = 0 ; i < 7 ; i++) 
    { 
   putchar(setup[i]); 
    } 
} 
// Sets channel period to 4 Hz (8192) 
void setchperiod (void) 
{ 
   uint8_t i; 
   uint8_t setup[9]; 
    
   setup[0] = 0xa4;   //sync 
   setup[1] = 0x03;   //Length = 3 (short needed, little endian) 
   setup[2] = 0x43;   //message ID = set channel period 
   setup[3] = 0x00;   //ch # 0 
   setup[4] = 0x92;   //Least significant byte of 8192 
   setup[5] = 0x81;   //Most significant byte of 8192 
   setup[6] = 0xf7;   //checksum 
   setup[7] = 0x00; // zero pad 
   setup[8] = 0x00; // zero pad 
    
   for(i = 0 ; i < 9 ; i++) 
    { 
   putchar(setup[i]); 
    } 
} 
// Sends Data=AAAAAAAAAAAAAAAA 
void send (void) 
{ 
   uint8_t i; 
   uint8_t setup[13]; 
    
   setup[0] = 0xa4;   //sync 
   setup[1] = 0x09;   //length = 9 bytes 
   setup[2] = 0x4e;   //message id = broadcast data 
   setup[3] = 0x00;   //ch # 0 
   setup[4] = 0xaa; 
   setup[5] = 0xaa; 
   setup[6] = 0xaa; 
   setup[7] = 0xaa; 
   setup[8] = 0xaa; 
   setup[9] = 0xaa; 
   setup[10] = 0xaa; 
   setup[11] = 0xaa; 
   setup[12] = 0xe3; 
    
   for(i = 0 ; i < 13 ; i++) 
    { 
   putchar(setup[i]); 
    } 
} 
void ioinit (void) 
{ 
    //1 = output, 0 = input 
    DDRB = 0b11101111; //PB4 = MISO 
    DDRC = 0b11111111; //all outputs 
    DDRD = 0b11111110; //PORTD (RX on PD0) 
    //USART Baud rate: 4800 
    UBRR0H = (MYUBRR >> 8); 
    UBRR0L = MYUBRR; 
    UCSR0B = (1<<RXEN0)|(1<<TXEN0); 
    
    stdout = &mystdout; //Required for printf init 
} 
static int uart_putchar(char c, FILE *stream) 
{ 
    if (c == '\n') uart_putchar('\r', stream); 
  
    loop_until_bit_is_set(UCSR0A, UDRE0); 
    UDR0 = c; 
    
    return 0; 
} 
uint8_t uart_getchar(void) 
{ 
    while( !(UCSR0A & (1<<RXC0)) ); 
    return(UDR0); 
} 
//General short delays 
void delay_ms(uint16_t x) 
{ 
  uint8_t y, z, w; 
  for ( ; x > 0 ; x--){ 
    for ( y = 0 ; y < 90; y++){               //was 90, 11 gives delayms(500) actually 500ms at 8MHz 
      for ( w = 0 ; w < 8; w++){            //New - put in to compensate for clock divide by 8 error in original 
         for ( z = 0 ; z < 6 ; z++){ 
            asm volatile ("nop"); 
      }          
      } 
    } 
  } 
}