I am new to this world of GPS’s.
The other day a fellow ham radio operator gave me four ET-102
GPS RECEIVER ENGINE BOARDs, along with 1 Trimble Active Antennas.
The ET-102 is identical to the GPS-00577 GPS unit.
Knowing little about GPS boards and how they are connected to my
home computer. So I started reading the Product guide that came with
the boards. I hooked one of the boards up to serial cable (DB9-M to
DB9-F) and made sure the computer can see the cable, and it did.
I mounted the GPS boards on a breadboard and wired the board to
a DB9-F with the following connections. pin 10 of GPS board to pin 5
of DB9-F, pin 11 of GPS board to pin 2 of DB9-F, pin 12 of GPS board
to pin 3 of DB9-F. Connected antenna to GPS board, and applied
5vdc (regulated) to pin 2 of GPS board.
Prior to doing the above, I download two programs that was told would
function with the ET-102/ER-102 board. They are GPS-INFO-V1.03
and SirFGPSTweaker. I loaded the programs into my computer and they
setup perfectly.
I then loaded/ran the GPS-INFO-V1.03 program and applied power to
the GPS board. I told the program to scan for port that the GPS board
and serial cable were using. It scanned both port 1 and 3, and came
back and said “NO DEVICE”.
At this point I also tried using a “serial to USB” cable and still no results.
My question is…
Is there something else that I didn’t connect, wire correctly?
I have other equipment that uses the USB ports, and they work perfectly.
Any help in getting these board hooked up correctly and working would
be appreciated, and any other information you need I can give to you.
Can post answer here or e-mail me at: wa6ddf@arrl.net.
RIMFIRE :roll: