Hi all,
Sys Info : Linux 2.6.8.1 and I am using Jffs2 file sys.
Hardw Info : I have 32M flash space to use.
Jffs2 Load code : fis create -d 0x800000 -l 0xa00000 jffs2
~ # cat /proc/mtd
dev: size erasesize name
mtd0: 00040000 00020000 “RedBoot”
mtd1: 00a00000 00020000 “jffs2”
mtd2: 00200000 00020000 “zImage”
mtd3: 00380000 00020000 “unallocated”
mtd4: 00001000 00020000 “RedBoot config”
mtd5: 00020000 00020000 “FIS directory”
~ # df -h
Filesystem Size Used Available Use% Mounted on
/dev/mtdblock1 10.0M 6.7M 3.3M 67% /
The question is :
I just want a Larger jffs2 size (may be 20m ) so that I can store more data(music). What can i do to Expand Jffs2 Size ?
Thanks for your help !
Best wishes ![]()
FengYi