I’m trying to build a robot car using the sparkfun auto phat. I want to use the external power header on the phat for the power and not usbc but it is not working. I am supplying 7.2v via 6 AA NiMH batteries but it is not working. The motors will not run. 7.2v is within the range specified on the board when connecting to MTR external power. I have connected gnd pin to my external power source gnd.
However the motors and pi will run when I use the auto phat’s usbc port, the same batteries work fine on a similar custom made robot car, the pins I have soldered to external power on the phat have clean connections and all work fine when tested in continuity mode with a multimeter.