I’m getting an error from the SFE DRC on files that pass the Freedfm chcker. How deo I find out what aperture 18 is? Current files are here:
http://home.comcast.net/~amcfall/zip.zip
The error is on the top copper. I get:
Checked Aperture 10 (0.059x0.05): Passed
Checked Aperture 11 (0.045x0.05): Passed
Checked Aperture 12 (0.085x0.01): Passed
Checked Aperture 13 (0.085x0.01): Passed
Checked Aperture 14 (0.043x0.08): Passed
Checked Aperture 15 (0.138x0.08): Passed
Checked Aperture 16 (0.051x0.05): Passed
Checked Aperture 17 (0.01): Passed
Checked Aperture 18 (0.00): Failed
        Error - Aperture too thin
Checked Aperture 19 (0.02): Passed
Checked Aperture 20 (0.04): Passed
Checked Aperture 21 (0.05): Passed
Checked Aperture 22 (0.03): Passed
Checked Aperture 23 (0.03): Passed
Everything passes the layer checker though. Sorry, I’m a nooob (but getting less so).
Avery
             
            
              
              
              
            
            
           
          
            
            
              If you open up your gerber file in notepad, you will see something like this:
G75*
G70*
%OFA0B0*%
%FSLAX24Y24*%
%IPPOS*%
%LPD*%
%AMOC8*
5,1,8,0,0,1.08239X$1,22.5*
%
%ADD10OC8,0.0600*%
%ADD11C,0.0100*%
%ADD12C,0.0300*%
%ADD13C,0.0160*%
%ADD14C,0.0150*%
D10*
X001514Y001534D03*
X002514Y001534D03*
X003514Y001534D03*
X004514Y001534D03*
The lines that say %ADD1(whatever) are the ones that specify aperatures. The number following the comma specifies the trace width in inches. Since Sparkfun has a lower limit of 8mils, if any of the numbers following the apperature definition smaller than 0.008, that means a trace has been defined which is smaller than the minimum that Spark fun can have manufactured reliably.
Open up your gerbers in viewmate to see what your board looks like. Then close everything and manually edit your gerbers and change any of the aperatures numbers less than 0.008 to 0.008. Then reopen your files in Viewmate to see what has changed and to make sure everything still fits.
Hope that helps!
-Bill
             
            
              
              
              
            
            
           
          
            
            
              o_O
There be a bug we says, lol.
%ADD10R,0.059X0.051*%
%ADD11R,0.045X0.055*%
%ADD12R,0.085X0.016*%
%ADD13R,0.085X0.016*%
%ADD14R,0.043X0.085*%
%ADD15R,0.138X0.085*%
%ADD16R,0.051X0.059*%
%ADD17C,0.010*%
%ADD18C,0.008*%
%ADD19C,0.020*%
%ADD20C,0.040*%
%ADD21C,0.050*%
%ADD22C,0.030*%
%ADD23C,0.036*%
for some reason its missing the last number from the apperture data. Just an offset problem (opps) I will fix this as soon as I find some time (possibly this afternoon).
Other than that, i can say this file does pass.
             
            
              
              
              
            
            
           
          
            
            
              Thank you!  I will send this one off to Ben.
 I will send this one off to Ben.
Avery
             
            
              
              
              
            
            
           
          
            
            
              ok fixed, i had an offset to removing formatting as $j rather than $j + 1. 30 Minutes for 4 characters (inc. Spaces). lol
             
            
              
              
              
            
            
           
          
            
            
              Awesome, she passes now. I’m so excited, my first passing set of gerber files!