Fingerprint Scanner - TTL (GT-521F52) touch IC and wake-up function

Hi,

Is it possible to operate the touch IC using the SDK Demo package in the hookup guide? I only have on hand the fingerprint scanner, a Qwiic cable, and an FTDI Basic Breakout - 3.3V. Can I operate the touch IC using only these items? Else, what boards would work with the touch IC? In addition, what interface does the touch IC use?

Thanks!

Is it possible to operate the touch IC using the SDK Demo package in the hookup guide?

I don't think the demo SDK is programmed to use the touch sensor.

I only have on hand the fingerprint scanner, a Qwiic cable, and an FTDI Basic Breakout - 3.3V. Can I operate the touch IC using only these items? Else, what boards would work with the touch IC? In addition, what interface does the touch IC use?

No the touch sensor is on it's own connector and that doesn't communicate through serial. It looks like a 2 wire interface similar to I2C but I don't think it's actually I2C. Sadly, I've not seen any code for the touch sensor but you would need a microcontroller to read it.