Hello all, I’ve finished a PCB that makes use of the Arduino, Sparkfun accelerometer (memsic 2125 i believe), a GSR sensor, RF modules from Sparkfun (315 Mhz), muscle wire output, and Soundgin mini-synth. Circuit schematic and PCB top copper / bottom copper is located here: http://tiny.cc/DvaaM.
I’m pretty confident about my board, I’ve done several designs before, although this is a more “complex” one I’ve done. I’ve double checked everything, made sure I’ve got nice power decoupling caps, fat traces on all power/gnd signals. Top layer is mostly power planes, bottom layer is mostly ground plane save the horizontal 3.7v signal. For power, I’m using 3.7v Li-On batteries that get boosted up to 5v for the whole circuit In addition, the 3.7v is used to power 4 pairs of muscle wires. It’s also going through a voltage reg to 1.5v for the GSR so I don’t have to use an external battery for that. What else… I’ve got loads of jumper pins that are mostly used to connect external stuff like batteries, sensors etc. If anyone wants to briefly look at schematics and give feedback that would be good.
One question though - does it make a difference if my power / gnd planes copper pours are thatched, like criss cross design? I’ve heard that it helps to dissipate heat or whatever… but I’m just going with a solid fill.
TIA