Following sparkfun BNO080 guide. Installed library but yet arduino cannot find file or directory. I am completely stuck and i havent even started ![]()
Yes, iāve installed it. still no luck
Looked everywhere for a fix. tried adding the sparkfun zip file too but that fails to add.
Faulty board?
That issue wouldnāt be the board itself. It seems like it is an issue on your software side of things. What version of Arduino IDE are you using?
Using the app version 1.8.33.0
https://www.youtube.com/watch?v=Wkyg_Mx ⦠e=youtu.be
Sorry about the bad quality! I know i must be missing something simple!
Iām unable to view the video, permissions are set to private. Also, the latest stable release of Arduino is [1.8.12. Iām not familiar with the version you are using, so it is highly possible that there are compatibility issues.](https://www.arduino.cc/en/Main/Software)
Installed it with installer rather than the app. still no luck there. correct its 1.8.12. ive made the video viewable now
Since youāve installed the SparkFun libraries can you run one of the example sketches under āFile>Examples>SparkFun BNO080 Cortex Based IMUā?
There isnt SparkFun BNO080 Cortex Based IMU in the examples. if you mean loading the sketch from the library options then no still says no file or destination ![]()
That is bizarre that there arenāt any examples since you do have the library installed through Arduinoās Library Manager. The examples show in mine.
You may have to uninstall all BNO080 libraries and files, then reinstall through the Arduino Library Manager. It may even require an re-installation of the Arduino IDE. Unfortunately, this error is on the Arduinoās IDE side. You may also want to visit Arduinoās Support Forum to see if other users have had these kinds of errors.
Finally got past it! i think i had to load them though the exmaple in aurdino and not open the file. But⦠Im now getting āBNO080 not detected at default I2C address. Check your jumpers and the hookup guide. Freezingā⦠Its a qwick connect⦠so i have no idea