i am trying to have my arduino send serial data at a baud rate of 250K.
but my mac osx does not have 250K as one of it’s standard baud rates.
i read about aliasing baud rates which is done by altering System/Library/Extensions/FTDIUSBSerialDriver.kext
http://www.dbpharrison.com/general/thermitrackdriver/
ftdi has also talks about this in it’s manual:
http://www.ftdichip.com/Support/Documen … Driver.pdf
but i am not sure which of the many listed device to change.
any advice?
thanks.
the Arduino’s UART and crystal frequency likely cannot run at 115200, nor higher. To run at these speeds, a crystal of 14.7456MHz is needed. Even so, higher than 115200 is unlikely.
Also, it may be that some of Arduino libraries are hard-coded for other than 14.7456MHz.
so far it is not a problem to receive data at the arduino from my computer at 250K.
i followed this tutorial and it works great
http://playground.arduino.cc//DMX/Ardmx
my setup is computer - enttect dmx device - rs485 chip - arduino. and it works.
but now i also want to send data back to my computer and don’t want to/ don’t know how to send it back through the same dmx device. so i thought to send it back through a sparkfun rs485 to usb adapter.
a work around would be to figure out how to send and receive at different speeds. for example tx at 9600 and rx at 250K