I found out that the LED is flashing in case of no fix.
But if the position fixed, the LED is on.
On mine the LED flashes when I have a fix, and is steady on when I don’t.
okay this is weird…
so i just left the thing plugged in… went off to do a few things… came back and the LED is blinking…
and now i’m getting data… it’s weird… because last night i would leave it alone for like 10 minutes… and it would never get a fix…
why is it doing it now??
Assuming you don’t have a loose connection somewhere on the GPS, that could be the result of a poor signal combined with a receiver that has out of date information. When first powered on, the receiver only knows where the satellites were when it left the factory, so it takes longer to find where the satellites are now. Once it finds one it should catch up pretty quickly as all the satellites send out approximate locations of the others.
Whn i switch to the sirf protocol… i get nothing in debug view…
i get something in the signal and radar views… i get nothing in the map view… in the radar view i get two little pictures… but that’s it…
That’s expected. The signal view box tells you what satellites you’re receiving from, and how strong the signal is. The radar box doesn’t give much data that the signal view box doesn’t. The map view box doesn’t update until you click the “Current as origin” button, then it will show you how much the gps position drifts (if the gps isn’t moving). It also gives you the gps location, quality of fix, and how many satellites were used.
i cna’t read the thing anymore…
Do you mean that you aren’t getting any output from the receiver, or that it isn’t getting a position fix? If you aren’t getting any output from the receiver you can try the “Synchronize Protocol & Baud Rate” under the “Action” menu in SiRFDemo. That should try to set the receiver to SiRF protocol at 57600bps. If that doesn’t work, do you get any output if you open the port under hyperterm or something similar? If you get data that looks random it may be set to a different baud rate than you’ve selected. Try the others. However, that may not be so since the SiRF Binary protocol looks pretty random in hyperterminal.
i’m trying to get data from it again… and now it can’t lock on to anything…
is this okay?? i guess i have to try different locations??
It’s odd that you would get a fix, then not be able to get one again. If it isn’t too much trouble, try to find a place that has as few obstructions between you and the sky as possible. If, after about 10 minutes, you don’t get any fix, I would talk to SFE about a return.