Hello everyone,
I would like some advice about connecting
SparkFun GM862 Evaluation Board - Basic 50-Pin
without any external microcontroller.
http://www.sparkfun.com/commerce/produc … cts_id=277
In the GM862 Evaluation Board - Basic 50-Pin,
I’m connecting :
-(the four) 3.8V pin, directly with power
(3,8 volts nominal, Min.3,4 volts, Max.4,2 volts,
and 2.5Amper. I’m using LM350T able to supply 3.0A)
-(the two) GND pin, to ground.
-GND/ADC pin, to ground.
what is that for??
then what about…
1)the ON/OFF pin ??
GM862-GPS Hardware User Guide on page 19 of 73 says :
“To turn on the GM862-GPS the pin ON# must be tied low for at least 1 second and then released”
what does “tied low” mean ??
does “tied low” mean connected to the ground??
Can i use a “Momentary Push Button Switch”
connecting the ON/OFF pin to the GROUND
to turn the module on??
Is that correct??
somewhere else in the web i noticed the expression “active low”
what does “active low” mean??
2)STATUS pin ??
I think i have to put a green led with 100R resistor connected to the ground.
and then depending of the status, le led stay on, off, or blinking.
Is that correct??
3)DTR pin??
considering the module is already programmed in python language and already tested
and doing his job pretty well. I don’t need to program it, i just need
the script execuption.
what about this pin??
what should i do with it??
somewhere else i read 2.8 Volts??
should i also supply 2.8 volts??
and just in case, what and when is using 2.8 volts??
Before connecting anything i would appreciate some advice
from who knowns better then me what is doing.
Thanks.Roberto.