Hello everyone here,
I have the following hardware :
1)SparkFun Electronics - GM862 Cellular Quad Band Module with GPS
http://www.sparkfun.com/commerce/produc … ts_id=7917
with Firmware version 07.03.400
- SparkFun Electronics - GM862 Evaluation Kit - USB
http://www.sparkfun.com/commerce/produc … cts_id=280
I want to make the GPS system portable. I have a high altitude ballon project, and using this GPS system to track where it is.
I know you can power the GM862 evaultion USB Board from the 5-9v dc sockect (PSU i am guessing) no? (or is it both usb and dc socket)?
It says that you can: Communication and power via USB. The USB chip can be disconnected to allow for external control of the TX and RX pins on the GM862 module (3V logic only!). I will not have USB ( or a computer) when the Payload is 30 km in the air, so what do i have to do to make the GM862 GPS module powered and working portably? Can it be done? Thanks. Scott
btw it mentions : Note: Some USB ports cannot source enough current to power the GM862 module. If the power supply is inadequate, the module may shut down while attempting to connect to the cellular network. An external power supply will correct this problem if it is experienced.
Does this effect me usingt he board portably (i.e not connected to a computer) Thanks.