I note on another thread here a command AT#CAMON, where is this documented?
Has anyone used the CMUX program? When I use it it never connects to the board, the Modem port just gives error-connecting-error forever.
How do you get pictures into the devices memory? Say from a camera??
Hello,
I also dont heard about that command.
You can check the process u following to connect CMUX carefully.
Otherwise the problem may be in your script which you want to execute.
Thanks,
velocet
3
The CMUX and all of the latest documentation can be downloaded here.
http://www.roundsolutions.co.uk/techdocs
A much better solution is to use the python debuger from roundsolutions, its a bit pricey but it works well.