I’m going to make a GP order soon for a breakout for a TI MSP uC. I’m not using the deal because the pitch on this particular package, 80LQFP, is JUST less than 8 mils. I’m just taking each pin straight to a header which will align with a breadboard. I have plenty of extra space on each board and since I will have many of these boards, I wanted to include other packages that could be hooked up to the same pinouts. I’ve already got a 64 QFP right inside the larger one since they fit together perfectly.
Obviously each board could only be used for one IC at a time since they’ll be sharing signals. So my question is… what other common packages should I include? I am set up to etch boards so I can do all the big ones but packages with pitch smaller than 15 mils get pretty messy… Any suggestions? Thanks!