Note: This is also posted in the Spark Fun Site Questions/Comments forum. I wasn’t getting any answers there so now I trying this location. ![]()
I’m just starting with the Data Logger. It seems to work fine with the default settings.
So, now I’m working through the instructions and it says I can set the messages it will log by setting the Mode to 1 in the in the GLOGCON.TXT file on the SD card. So I set the following configuration where I only changed the mode from 0 to 1 everything else is default:
Mode = 1
Log What = RMC;GGA;GSA
Time Between Logs = 00:10:00
Holdoff = 5
now I get a solid blue LED on the logger board and nothing is logged.
Anybody know what I am doing wrong?
HELP!
Mike