GPS Logger v2.4

Just starting with the Data Logger. It seems to work fine with the default settings. So, I’m working through the instructions and it says I can set the messages it will log by setting the Mode to 1 in the in the GLOGCON.TXT file on the SD card. So I set the following configuration where I only changed the mode from 0 to 1 everything else is default:

Mode = 1

Log What = RMC;GGA;GSA

Time Between Logs = 00:10:00

Holdoff = 5

now I get a solid blue LED on the logger board and nothing is logged.

Anybody know what I am doing wrong?

HELP!

Mike