GPS-RTK Raspberry Pi pHAT issues.

Hello,

I just connected my pHAT for the first time and ran the example program and was able to receive Lat., Long. correctly. I am not trying to connect a correction source to the system yet. But when I went into u-Center software, I updated the Firmware to the latest ZED-F9P firmware from ublox’s website. The firmware update was successful according to the log, but after the update I am no longer able to see the connection to the COM port (bottom right “COM# + Baudrate” flashing green) anymore or when I run the same example that just returned the coordinates, nothing is received.

Is this a configuration file issue? Is there a default configuration file that comes on the Sparkfun ZED-F9P boards and when you do the firmware update it will wipe it?

Please let me know if you can help or if anyone else has had this issue.

Thanks.

Thanks for reaching out to us on this.

It is most likely an issue with the COM port being incorrectly assigned by the OS after the update; try viewing the Device Manager on your OS and view the COM ports…then unplug and re-plug the board, the device that disappears and then re-appears when you plug ti back in should be the correct one for your device. Then change settings in u-Center to match

If that doesn’t work, try reinstalling the drivers (different board used in example, but similar process): https://learn.sparkfun.com/tutorials/ge … ll-drivers

Hope this helps, and happy sparking!

Thanks for the reply, TS-Russell.

The computer is able to recognize the board after the update and even shows in the same COM5 slot that I had it in prior to the update. In u-center I can even select the COM5 from the connection drop down menu.

Also, how would a Windows OS driver issue affect the pHAT when it’s disconnected from the PC and is still unable to receive/ record data values?

We’ll be investigating further on whether the firmware update is causing conflicts; for now I would advise reverting back to the old/functional firmware until we have something more to offer.

Have a great day!

I tried reverting backwards and it was successful but the issue persisted on both u-center and the .py example. That’s what made me think it had to be something in the configuration set up or something. Keep me posted!

Hello,

I noticed this article was published!

https://learn.sparkfun.com/tutorials/ho … s-receiver

Is there a way that you all can share the ZED-F9P Config.Txt that is shown in the tutorial? Or the exact pHAT config.txt if it varies at all from the other ZED-F9P boards? I can try to load it back on and see if that helps.

What product are you using? GPS-RTK Raspberry Pi pHAT is in the subject but you’re asking about a configuration file for the ZED-F9P?

I’m not seeing anything in the guide about a config.txt file, where are you getting that?