GPS-RTK-SMA Breakout - ZED-F9P Detect Insufficient Power

Hi,

I am using two of these modules:

https://www.sparkfun.com/products/16481

Is there a way to detect if the power supplied via USB is not sufficient?

There is no mention of this in the Hookup Guide (link below)

https://learn.sparkfun.com/tutorials/gp … 1652952966

I think you can use this one: https://www.amazon.com/Eversame-Multime … ljaz10cnVl

I always keep on hand one of the USB current meters that tepalia02 mentioned. Very handy.

And I just happen to have hardware to get actual readings. ZED-F9P + u-blox antenna:

https://cdn.sparkfun.com/assets/learn_t … tion_1.jpg

~120mA with no SIV (acquisition). This matches the datasheet specs pretty well:

https://cdn.sparkfun.com/assets/learn_t … mption.jpg

Running two ZEDs with active antennas off a USB port shouldn’t get above 250mA and should be well under the 500mA limit of any given USB port.