Hi,
I recently received my SparkFun GPS-RTK-SMA Breakout (GPS-16481) and GNSS Multi-Band Magnetic Mount Antenna (GPS-15192).
When I went to connect the antenna to the board, I quickly realized I had a problem. Both the antenna and the breakout SMA connectors were male. (I’ve attached an image of the SMA connectors)
The male pin on the antenna matches the images shown on the product page for it.
I read through the product page of the breakout, through the schematic, and through the hookup guide. Curiously, I couldn’t find a conclusive answer to whether the SMA connector on the breakout was intended to be male or female. I even watched the YouTube video hoping to see a glance of the inside of the SMA connector.
While the antenna is included in the listed hookup accessories of the breakout, no special SMA adapters are.
The GPS-RTK2 Hookup Guide does mention that if an additional SMA connector is needed for PPS pin of the breakout, the female SMA connector (WRL-00593) is suggested.
With all this considered, my guess is that the SMA connector on the breakout was supposed to be female but somehow swapped for a male.
Is anyone able to verify whether the SMA connector of the GPS-RTK-SMA Breakout is female or male?
Thank you,
Dave