Hacking infrared oven for PCB reflow

Hi,

I got a little 20L oven with a temp controller in order to reflow PCB but the temp does not increase enough fast :-/

I found this type of infrared (halogen) forced convection oven :

http://www.nuwaveoven.com/nuwave-infrar … ssic.asp#1

There’s a lot of similar oven for $35 on the web :

http://www.rueducommerce.fr/m/ps/mpid:M … 0BM7028933

The volume is low , 1500W power, and it seems to cook pretty fast.

Do you think it’s possible to hack it for reflowing ?

I like the idea of glass in order ton control the process. And the form factor is cool :lol:

Finally I got a little one , mod it an did some tests .

I got this with a simple on/off regulation witn an arduino and a max6675

http://img705.imageshack.us/img705/5183/profiledi.png

I thinks this type of oven is really good for prototyping . I have to make final test with a PCB .Probably next month .

You can read more on my blog :

http://www.tronique.fr

(it’s in french but google trad is ok ! :slight_smile: )

I use an older Black & Decker Toast R Oven for my prototyping. I have run across people using IR ovens. They do get hotter, faster. The thing is, an IR oven will heat the board but not the air around it. So how do you measure the temp of the board while its cooking? You need to be able to do that in order to maintain a proper reflow temp profile.

With a conventional or convetion over you can measure the air temp. While that is not ideal, since you really do want to know the board temp, its at least easy to do.

I use the oven congroller sold here by SparkFun. It was easy to build and it comes with the software. Not that its hard to do it yourself of course.

with this oven and other IR cooker, the IR don’t hit the board directly because there’s an inox plate (with some holes but not directly under the bulb) below the bulb . The fan inside the perimeter of the bulb push the hot air on the side for the little cyclonic effect. The plate probably radiate some IR too, But I guess it’s more a convection oven than an IR one due to this structure . (I’ll post some pictures later).

For the temperature measures, the thermocouple is below the plate at the middle, where the PCB is supposed to be placed. To limit the possible IR effect, I put some aluminium tape just above the thermocouple like a umbrella. So it’s the temperature of the air that is measured.