Help Flash Programmin the SAM7-p256

We are trying to program the SAM7-p256 using the ARM USB OCD. We can write to the chip using a debug version but the code does not run after being written to the MCU. The Olimex flashes and the board does not blink. If we remove the jtag connector and replace it the code starts to run.

We are using eclipse and all the other software from the CD that came with the ARM USB OCD.

We are wondering how to create a release version that will run without communication from the ARM USB OCD.