Hi there! I’m almost finished with this code for my LED clock, but I’m running into an issue attempting to use buttons to set the time. I can “set” it, but the changes don’t kick back in unless I reopen the serial monitor. As in, if I turn on the “set time” button, then add five hours and turn off the “set time” button, changes don’t reflect until I open serial monitor. I want the changes to reflect when the “set time” button is released. Also, my code doesn’t seem to be looping (it only reads the time once in serial monitor). Could someone help me figure out what’s wrong? I’d greatly appreciate it!! ![]()
#include <Wire.h> // specify use of Wire.h library.
#include <Time.h>
#include <DS1307RTC.h>
#define ONE_HZ_SW 1 // one Hz square wave from Ds1307
#define blinkPin 13
#define Sw0 4
#define Sw1 5
#define Sw2 6
int hrPins[] = {52, 50, 48, 46, 44, 42, 40, 38, 36, 34, 32, 30};
int minPins[] = {31, 53, 51, 49, 47, 45, 43, 41, 39, 37, 35, 33};
void setup()
{
tmElements_t tm;
Wire.begin(); // join i2c bus (address optional for master)
Serial.begin(9600);
digitalWrite(blinkPin, 0);
pinMode(ONE_HZ_SW, INPUT_PULLUP);
pinMode(Sw0, INPUT_PULLUP); // for this use a slide switch
pinMode(Sw1, INPUT_PULLUP); // N.O. push button switch
pinMode(Sw2, INPUT_PULLUP); // N.O. push button switch
Serial.println("DS1307RTC Read Test");
Serial.println("-------------------");
}
void loop()
{
tmElements_t tm;
// wait or HIGH
while (!digitalRead(ONE_HZ_SW))
{
}
if (RTC.read(tm)) {
Serial.print("Ok, Time = ");
print2digits(tm.Hour);
Serial.write(':');
print2digits(tm.Minute);
Serial.write(':');
print2digits(tm.Second);
Serial.print(", Date (D/M/Y) = ");
Serial.print(tm.Day);
Serial.write('/');
Serial.print(tm.Month);
Serial.write('/');
Serial.print(tmYearToCalendar(tm.Year));
Serial.println();
}
else
{
if (RTC.chipPresent())
{
Serial.println("The DS1307 is stopped. Please run the SetTime");
Serial.println("example to initialize the time and begin running.");
Serial.println();
}
else
{
Serial.println("DS1307 read error! Please check the circuitry.");
Serial.println();
}
delay(9000);
}
delay(1000);
tm.Hour = (tm.Hour + 11) % 12; // This maps 0 to 11 (all on), 1 to 0 (only first on), 11 to 10 (all but last on), 12 to 11 (all on), 13 to 0 (first on), 23 to 10 (all but last on)
for (int i = 0; i < 12; i++)
{
digitalWrite(hrPins[i], tm.Hour >= i);
tm.Minute /= 5; // We only care about the time in 5-minute increments
}
for (int i = 1; i < 12; i++)
{
digitalWrite(minPins[i], tm.Minute >= i);
digitalWrite(minPins[0], tm.Minute == 0); // The first pin behaves differently: it only turns on during the first 5 minutes
}
if (!(digitalRead(Sw0))) set_time(); // hold the switch to set time
while (digitalRead(ONE_HZ_SW))
{
}// wait for low
toggle(blinkPin);
}
void print2digits(int number) {
if (number >= 0 && number < 10) {
Serial.write('0');
}
Serial.print(number);
}
// toggle the state on a pin
void toggle(int pinNum)
{
int pinState = digitalRead(pinNum);
pinState = !pinState;
digitalWrite(pinNum, pinState);
}
void set_time() {
byte minutes = 0;
byte hours = 0;
while (!digitalRead(Sw0)) // set time switch must be released to exit
{
while (!digitalRead(Sw1)) // set minutes
{
minutes++;
if ((minutes & 0x0f) > 9) minutes = minutes + 6;
if (minutes > 0x59) minutes = 0;
Serial.print("Minutes = ");
if (minutes >= 9) Serial.print("0");
Serial.println(minutes, HEX);
delay(250);
}
while (!digitalRead(Sw2)) // set hours
{
hours++;
if ((hours & 0x0f) > 9) hours = hours + 6;
if (hours > 0x23) hours = 0;
Serial.print("Hours = ");
if (hours <= 9) Serial.print("0");
Serial.println(hours, HEX);
delay(250);
}
Wire.beginTransmission(0x68); // activate DS1307
Wire.write(0); // where to begin
Wire.write(0x00); //seconds
Wire.write(minutes); //minutes
Wire.write(0x80 | hours); //hours (24hr time)
Wire.write(0x06); // Day 01-07
Wire.write(0x16); // Date 0-31
Wire.write(0x11); // month 0-12
Wire.write(0x13); // Year 00-99
Wire.write(0x10); // Control 0x10 produces a 1 HZ square wave on pin 7.
Wire.endTransmission();
}
}