Dear all,
problems>
1)When i working with DS1307 . I found that time has hanged at particular time. Is it possible to avoid hang operation through software. I have used external reset pin to reset RTC it worked. But i wanna know whether it possible to reset via software.If any changes to be made in below code let me know
2)while uploading below program, i found that date and time not get set properly . Let me know the reason for behaviour of RTC.
example code for rtc write given below.
#include"Wire.h"
#define DS1307_ADDRESS 0x68
byte zero = 0x00; //workaround for issue #527
void setup(){
  Wire.begin();
  Serial.begin(9600);
 // rtc.Set_Time(13,36,0);
  // rtc.Set_Date(2013,3,4);
 setDateTime(); //MUST CONFIGURE IN FUNCTION
}
void loop(){
  
  printDate();
  delay(1000);
}
void setDateTime(){
  byte second =45; //0-59
  byte minute =59; //0-59
  byte hour =12; //0-23
  byte monthDay =12; //1-31
  byte month =3; //1-12
  byte year  =13; //0-99
 
 Wire.beginTransmission(DS1307_ADDRESS);
  Wire.write(zero); //stop Oscillator
  Wire.write(decToBcd(second));
  Wire.write(decToBcd(minute));
  Wire.write(decToBcd(hour));
  
  Wire.write(decToBcd(monthDay));
  Wire.write(decToBcd(month));
  Wire.write(decToBcd(year));
  Wire.write(zero); //start
  Wire.endTransmission();
}
byte decToBcd(byte val){
// Convert normal decimal numbers to binary coded decimal
  return ( (val/10*16) + (val%10) );
}
byte bcdToDec(byte val)  {
// Convert binary coded decimal to normal decimal numbers
  return ( (val/16*10) + (val%16) );
}
void printDate(){
  // Reset the register pointer
  Wire.beginTransmission(DS1307_ADDRESS);
 
  Wire.write(0);
  Wire.endTransmission();
  Wire.requestFrom(DS1307_ADDRESS,7);
   int second = bcdToDec(Wire.read());
  int minute = bcdToDec(Wire.read());
  int hour = bcdToDec(Wire.read() & 0b111111); //24 hour time
  int monthDay = bcdToDec(Wire.read());
  int month = bcdToDec(Wire.read());
  int year = bcdToDec(Wire.read());
 /*  int second = 11;
  int minute =18;
  int hour = 18;
  int weekDay = 1;
  int monthDay = 2;
  int month = 11;
  int year = 12;
*/
  //print the date EG   3/1/11 23:59:59
  Serial.print(monthDay);
  Serial.print("/");
  
  
  Serial.print(month);
  Serial.print("/");
  
  Serial.print(year);
  Serial.print(" ");
  Serial.print(hour);
  Serial.print(":");
  Serial.print(minute);
  Serial.print(":");
  Serial.println(second);
}