i got a problem i can not Initialization display SSD1351 but now i can see something on display SSD1351, but itβs look like error. i think the command while i Initialization is wrong. could you give some advices to me. i connected it in 8-bit 80XX Parallel BS0=0; BS1=1 thank you a lot for helping me .
^ ^
:o
this is my code
#define DC1 GPIO_SetBits(GPIOC, GPIO_Pin_0);
#define DC0 GPIO_ResetBits(GPIOC, GPIO_Pin_0);
#define CS1 GPIO_SetBits(GPIOC, GPIO_Pin_1);
#define CS0 GPIO_ResetBits(GPIOC, GPIO_Pin_1);
#define WR1 GPIO_SetBits(GPIOC, GPIO_Pin_2);
#define WR0 GPIO_ResetBits(GPIOC, GPIO_Pin_2);
#define RES1 GPIO_SetBits(GPIOC, GPIO_Pin_3);
#define RES0 GPIO_ResetBits(GPIOC, GPIO_Pin_3);
void LCD_IO_init_out(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA , ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1| GPIO_Pin_2| GPIO_Pin_3| GPIO_Pin_4| GPIO_Pin_5| GPIO_Pin_6| GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
}
void LCD_IO_init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
//IO_control
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC , ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1| GPIO_Pin_2| GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
void Write_Command(unsigned char Data)
{
DC0
CS0
WR0
GPIO_Write(GPIOA,Data);
WR1
CS1
DC1
}
void Write_Data(unsigned char Data)
{
DC1
CS0
WR0
GPIO_Write(GPIOA,Data);
WR1
CS1
DC1
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Instruction Setting
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Set_Column_Address(unsigned char a, unsigned char b)
{
Write_Command(0x15); // Set Column Address
Write_Data(a); // Default => 0x00 (Start Address)
Write_Data(b); // Default => 0x7F (End Address)
}
void Set_Row_Address(unsigned char a, unsigned char b)
{
Write_Command(0x75); // Set Row Address
Write_Data(a); // Default => 0x00 (Start Address)
Write_Data(b); // Default => 0x7F (End Address)
}
void Set_Write_RAM()
{
Write_Command(0x5C); // Enable MCU to Write into RAM
}
void Set_Read_RAM()
{
Write_Command(0x5D); // Enable MCU to Read from RAM
}
void Set_Remap_Format(unsigned char d)
{
Write_Command(0xA0); // Set Re-Map / Color Depth
Write_Data(d); // Default => 0x40
// Horizontal Address Increment
// Column Address 0 Mapped to SEG0
// Color Sequence: A => B => C
// Scan from COM0 to COM[N-1]
// Disable COM Split Odd Even
// 65,536 Colors
}
void Set_Start_Line(unsigned char d)
{
Write_Command(0xA1); // Set Vertical Scroll by RAM
Write_Data(d); // Default => 0x00
}
void Set_Display_Offset(unsigned char d)
{
Write_Command(0xA2); // Set Vertical Scroll by Row
Write_Data(d); // Default => 0x60
}
void Set_Display_Mode(unsigned char d)
{
Write_Command(0xA4|d); // Set Display Mode
// Default => 0xA6
// 0xA4 (0x00) => Entire Display Off, All Pixels Turn Off
// 0xA5 (0x01) => Entire Display On, All Pixels Turn On at GS Level 63
// 0xA6 (0x02) => Normal Display
// 0xA7 (0x03) => Inverse Display
}
void Set_Function_Selection(unsigned char d)
{
Write_Command(0xAB); // Function Selection
Write_Data(d); // Default => 0x01
// Enable Internal VDD Regulator
// Select 8-bit Parallel Interface
}
void Set_Display_On_Off(unsigned char d)
{
Write_Command(0xAE|d); // Set Display On/Off
// Default => 0xAE
// 0xAE (0x00) => Display Off (Sleep Mode On)
// 0xAF (0x01) => Display On (Sleep Mode Off)
}
void Set_Phase_Length(unsigned char d)
{
Write_Command(0xB1); // Phase 1 (Reset) & Phase 2 (Pre-Charge) Period Adjustment
Write_Data(d); // Default => 0x82 (8 Display Clocks [Phase 2] / 5 Display Clocks [Phase 1])
// D[3:0] => Phase 1 Period in 5~31 Display Clocks
// D[7:4] => Phase 2 Period in 3~15 Display Clocks
}
void Set_Display_Enhancement(unsigned char d)
{
Write_Command(0xB2); // Display Enhancement
Write_Data(d); // Default => 0x00 (Normal)
Write_Data(0x00);
Write_Data(0x00);
}
void Set_Display_Clock(unsigned char d)
{
Write_Command(0xB3); // Set Display Clock Divider / Oscillator Frequency
Write_Data(d); // Default => 0x00
// A[3:0] => Display Clock Divider
// A[7:4] => Oscillator Frequency
}
void Set_VSL(unsigned char d)
{
Write_Command(0xB4); // Set Segment Low Voltage
Write_Data(0xA0|d); // Default => 0xA0
// 0xA0 (0x00) => Enable External VSL
// 0xA2 (0x02) => Enable Internal VSL (Kept VSL Pin N.C.)
Write_Data(0xB5);
Write_Data(0x55);
}
void Set_GPIO(unsigned char d)
{
Write_Command(0xB5); // General Purpose IO
Write_Data(d); // Default => 0x0A (GPIO Pins output Low Level.)
}
void Set_Precharge_Period(unsigned char d)
{
Write_Command(0xB6); // Set Second Pre-Charge Period
Write_Data(d); // Default => 0x08 (8 Display Clocks)
}
void Set_Precharge_Voltage(unsigned char d)
{
Write_Command(0xBB); // Set Pre-Charge Voltage Level
Write_Data(d); // Default => 0x17 (0.50*VCC)
}
void Set_VCOMH(unsigned char d)
{
Write_Command(0xBE); // Set COM Deselect Voltage Level
Write_Data(d); // Default => 0x05 (0.82*VCC)
}
void Set_Contrast_Color(unsigned char a, unsigned char b, unsigned char c)
{
Write_Command(0xC1); // Set Contrast Current for Color A, B, C
Write_Data(a); // Default => 0x8A (Color A)
Write_Data(b); // Default => 0x51 (Color B)
Write_Data(c); // Default => 0x8A (Color C)
}
void Set_Master_Current(unsigned char d)
{
Write_Command(0xC7); // Master Contrast Current Control
Write_Data(d); // Default => 0x0F (Maximum)
}
void Set_Multiplex_Ratio(unsigned char d)
{
Write_Command(0xCA); // Set Multiplex Ratio
Write_Data(d); // Default => 0x7F (1/128 Duty)
}
void Set_Command_Lock(unsigned char d)
{
Write_Command(0xFD); // Set Command Lock
Write_Data(d); // Default => 0x12
// 0x12 => Driver IC interface is unlocked from entering command.
// 0x16 => All Commands are locked except 0xFD.
// 0xB0 => Command 0xA2, 0xB1, 0xB3, 0xBB & 0xBE are inaccessible.
// 0xB1 => All Commands are accessible.
}
//=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Graphic Acceleration (Partial or Full Screen)
//
// a: Column Address of Start
// b: Column Address of End
// c: Row Address of Start
// d: Row Address of End
// e: Line Width
// f: Line Color - RRRRRGGG
// g: Line Color - GGGBBBBB
//=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Draw_Rectangle(unsigned char a, unsigned char b, unsigned char c, unsigned char d, unsigned char e, unsigned char f, unsigned char g)
{
unsigned char i,j;
Set_Column_Address(a,b);
Set_Row_Address(c,(c+e-1));
Set_Write_RAM();
for(i=0;i<(b-a+1);i++)
{
for(j=0;j<e;j++)
{
Write_Data(f); // Line Color - RRRRRGGG
Write_Data(g); // Line Color - GGGBBBBB
}
}
Set_Column_Address((b-e+1),b);
Set_Row_Address(c,d);
Set_Write_RAM();
for(i=0;i<(d-c+1);i++)
{
for(j=0;j<e;j++)
{
Write_Data(f); // Line Color - RRRRRGGG
Write_Data(g); // Line Color - GGGBBBBB
}
}
Set_Column_Address(a,b);
Set_Row_Address((d-e+1),d);
Set_Write_RAM();
for(i=0;i<(b-a+1);i++)
{
for(j=0;j<e;j++)
{
Write_Data(f); // Line Color - RRRRRGGG
Write_Data(g); // Line Color - GGGBBBBB
}
}
Set_Column_Address(a,(a+e-1));
Set_Row_Address(c,d);
Set_Write_RAM();
for(i=0;i<(d-c+1);i++)
{
for(j=0;j<e;j++)
{
Write_Data(f); // Line Color - RRRRRGGG
Write_Data(g); // Line Color - GGGBBBBB
}
}
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Show Regular Pattern (Full Screen)
//
// a: RRRRRGGG
// b: GGGBBBBB
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Fill_RAM(unsigned char a, unsigned char b)
{
unsigned char i,j;
Set_Column_Address(0x00,0x7F);
Set_Row_Address(0x00,0x7F);
Set_Write_RAM();
for(i=0;i<128;i++)
{
for(j=0;j<128;j++)
{
Write_Data(a);
Write_Data(b);
}
}
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Show Regular Pattern (Partial or Full Screen)
//
// a: Column Address of Start
// b: Column Address of End
// c: Row Address of Start
// d: Row Address of End
// e: RRRRRGGG
// f: GGGBBBBB
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Fill_Block(unsigned char a, unsigned char b, unsigned char c, unsigned char d, unsigned char e, unsigned char f)
{
unsigned char i,j;
Set_Column_Address(a,b);
Set_Row_Address(c,d);
Set_Write_RAM();
for(i=0;i<(d-c+1);i++)
{
for(j=0;j<(b-a+1);j++)
{
Write_Data(e);
Write_Data(f);
}
}
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Show Checkboard (Full Screen)
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Checkerboard()
{
unsigned char i,j;
Set_Column_Address(0x00,0x7F);
Set_Row_Address(0x00,0x7F);
Set_Write_RAM();
for(i=0;i<64;i++)
{
for(j=0;j<64;j++)
{
Write_Data(0xFF);
Write_Data(0xFF);
Write_Data(0x00);
Write_Data(0x00);
}
for(j=0;j<64;j++)
{
Write_Data(0x00);
Write_Data(0x00);
Write_Data(0xFF);
Write_Data(0xFF);
}
}
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Show Color Bar (Full Screen)
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Rainbow()
{
// White => Column 1~16
Fill_Block(0x00,0x0F,0x00,Max_Row,0xFF,0xFF);
// Yellow => Column 17~32
Fill_Block(0x10,0x1F,0x00,Max_Row,0xFF,0xE0);
// Purple => Column 33~48
Fill_Block(0x20,0x2F,0x00,Max_Row,0xF8,0x1F);
// Cyan => Column 49~64
Fill_Block(0x30,0x3F,0x00,Max_Row,0x07,0xFF);
// Red => Column 65~80
Fill_Block(0x40,0x4F,0x00,Max_Row,0xF8,0x00);
// Green => Column 81~96
Fill_Block(0x50,0x5F,0x00,Max_Row,0x07,0xE0);
// Blue => Column 97~112
Fill_Block(0x60,0x6F,0x00,Max_Row,0x00,0x1F);
// Black => Column 113~128
Fill_Block(0x70,Max_Column,0x00,Max_Row,0x00,0x00);
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Automatic Horizontal Scrolling (Instruction)
//
// a: Scrolling Direction
// β0x00β (Rightward)
// β0x01β (Leftward)
// b: Set Numbers of Column Scroll per Step
// c: Set Row Address of Start
// d: Set Numbers of Row to Be Scrolled
// e: Set Time Interval between Each Scroll Step in Terms of Frame Frequency
// f: Delay Time
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Horizontal_Scroll(unsigned char a, unsigned char b, unsigned char c, unsigned char d, unsigned char e, unsigned char f)
{
Write_Command(0x96); // Horizontal Scroll Setup
Write_Data((a<<7)|b);
Write_Data(c);
Write_Data(d);
Write_Data(0x00);
Write_Data(e);
Write_Command(0x9F); // Activate Horizontal Scroll
Delay(f);
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Vertical Scrolling (Full Screen)
//
// a: Scrolling Direction
// β0x00β (Upward)
// β0x01β (Downward)
// b: Set Numbers of Row Scroll per Step
// c: Set Time Interval between Each Scroll Step
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Vertical_Scroll(unsigned char a, unsigned char b, unsigned char c)
{
unsigned int i,j;
switch(a)
{
case 0:
for(i=0;i<128;i+=b)
{
Set_Start_Line(i);
for(j=0;j<c;j++)
{
Delay(200);
}
}
break;
case 1:
for(i=0;i<128;i+=b)
{
Set_Start_Line(128-i);
for(j=0;j<c;j++)
{
Delay(200);
}
}
break;
}
Set_Start_Line(0x00);
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Deactivate Scrolling (Full Screen)
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Deactivate_Scroll()
{
Write_Command(0x9E); // Deactivate Scrolling
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Fade In (Full Screen)
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Fade_In()
{
unsigned int i;
Set_Display_On_Off(0x01);
for(i=0;i<(Brightness+1);i++)
{
Set_Master_Current(i);
Delay(200);
}
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Fade Out (Full Screen)
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Fade_Out()
{
unsigned int i;
for(i=(Brightness+1);i>0;iβ)
{
Set_Master_Current(i-1);
Delay(200);
}
Set_Display_On_Off(0x00);
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Sleep Mode
//
// β0x00β Enter Sleep Mode
// β0x01β Exit Sleep Mode
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Sleep(unsigned char a)
{
switch(a)
{
case 0:
Set_Display_On_Off(0x00);
Set_Display_Mode(0x01);
break;
case 1:
Set_Display_Mode(0x02);
Set_Display_On_Off(0x01);
break;
}
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Connection Test
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Test()
{
unsigned char i;
RES0
for(i=0;i<200;i++)
{
Delay(200);
}
RES1
Set_Display_Mode(0x01); // Entire Display On Mode (0x00/0x01/0x02/0x03)
while(1)
{
Set_Display_On_Off(0x01); // Display On (0x00/0x01)
Delay(2);
Set_Display_On_Off(0x00); // Display Off (0x00/0x01)
Delay(2);
}
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Gray Scale Table Setting (Full Screen)
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Set_Gray_Scale_Table()
{
Write_Command(0xB8);
Write_Data(0x02); // Gray Scale Level 1
Write_Data(0x03); // Gray Scale Level 2
Write_Data(0x04); // Gray Scale Level 3
Write_Data(0x05); // Gray Scale Level 4
Write_Data(0x06); // Gray Scale Level 5
Write_Data(0x07); // Gray Scale Level 6
Write_Data(0x08); // Gray Scale Level 7
Write_Data(0x09); // Gray Scale Level 8
Write_Data(0x0A); // Gray Scale Level 9
Write_Data(0x0B); // Gray Scale Level 10
Write_Data(0x0C); // Gray Scale Level 11
Write_Data(0x0D); // Gray Scale Level 12
Write_Data(0x0E); // Gray Scale Level 13
Write_Data(0x0F); // Gray Scale Level 14
Write_Data(0x10); // Gray Scale Level 15
Write_Data(0x11); // Gray Scale Level 16
Write_Data(0x12); // Gray Scale Level 17
Write_Data(0x13); // Gray Scale Level 18
Write_Data(0x15); // Gray Scale Level 19
Write_Data(0x17); // Gray Scale Level 20
Write_Data(0x19); // Gray Scale Level 21
Write_Data(0x1B); // Gray Scale Level 22
Write_Data(0x1D); // Gray Scale Level 23
Write_Data(0x1F); // Gray Scale Level 24
Write_Data(0x21); // Gray Scale Level 25
Write_Data(0x23); // Gray Scale Level 26
Write_Data(0x25); // Gray Scale Level 27
Write_Data(0x27); // Gray Scale Level 28
Write_Data(0x2A); // Gray Scale Level 29
Write_Data(0x2D); // Gray Scale Level 30
Write_Data(0x30); // Gray Scale Level 31
Write_Data(0x33); // Gray Scale Level 32
Write_Data(0x36); // Gray Scale Level 33
Write_Data(0x39); // Gray Scale Level 34
Write_Data(0x3C); // Gray Scale Level 35
Write_Data(0x3F); // Gray Scale Level 36
Write_Data(0x42); // Gray Scale Level 37
Write_Data(0x45); // Gray Scale Level 38
Write_Data(0x48); // Gray Scale Level 39
Write_Data(0x4C); // Gray Scale Level 40
Write_Data(0x50); // Gray Scale Level 41
Write_Data(0x54); // Gray Scale Level 42
Write_Data(0x58); // Gray Scale Level 43
Write_Data(0x5C); // Gray Scale Level 44
Write_Data(0x60); // Gray Scale Level 45
Write_Data(0x64); // Gray Scale Level 46
Write_Data(0x68); // Gray Scale Level 47
Write_Data(0x6C); // Gray Scale Level 48
Write_Data(0x70); // Gray Scale Level 49
Write_Data(0x74); // Gray Scale Level 50
Write_Data(0x78); // Gray Scale Level 51
Write_Data(0x7D); // Gray Scale Level 52
Write_Data(0x82); // Gray Scale Level 53
Write_Data(0x87); // Gray Scale Level 54
Write_Data(0x8C); // Gray Scale Level 55
Write_Data(0x91); // Gray Scale Level 56
Write_Data(0x96); // Gray Scale Level 57
Write_Data(0x9B); // Gray Scale Level 58
Write_Data(0xA0); // Gray Scale Level 59
Write_Data(0xA5); // Gray Scale Level 60
Write_Data(0xAA); // Gray Scale Level 61
Write_Data(0xAF); // Gray Scale Level 62
Write_Data(0xB4); // Gray Scale Level 63
}
void Set_Linear_Gray_Scale_Table()
{
Write_Command(0xB9); // Default
}
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// Show Pattern (Partial or Full Screen)
//
// a: Column Address of Start
// b: Column Address of End
// c: Row Address of Start
// d: Row Address of End
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
void Show_64k_Pattern(unsigned char *Data_Pointer, unsigned char a, unsigned char b, unsigned char c, unsigned char d)
{
unsigned char *Src_Pointer;
unsigned char i,j;
Src_Pointer=Data_Pointer;
Set_Column_Address(a,b);
Set_Row_Address(c,d);
Set_Write_RAM();
for(i=0;i<(d-c+1);i++)
{
for(j=0;j<(b-a+1);j++)
{
Write_Data(*Src_Pointer);
Src_Pointer++;
Write_Data(*Src_Pointer);
Src_Pointer++;
}
}
}
void Show_256k_Pattern(unsigned char *Data_Pointer, unsigned char a, unsigned char b, unsigned char c, unsigned char d)
{
unsigned char *Src_Pointer;
unsigned char i,j;
Src_Pointer=Data_Pointer;
Set_Column_Address(a,b);
Set_Row_Address(c,d);
Set_Write_RAM();
for(i=0;i<(d-c+1);i++)
{
for(j=0;j<(b-a+1);j++)
{
Write_Data(*Src_Pointer);
Src_Pointer++;
Write_Data(*Src_Pointer);
Src_Pointer++;
Write_Data(*Src_Pointer);
Src_Pointer++;
}
}
}
void OLED_Init()
{
unsigned char i;
RES0
Delay(200);
RES1
Set_Command_Lock(0x12); // Unlock Driver IC (0x12/0x16/0xB0/0xB1)
Set_Command_Lock(0xB1); // Unlock All Commands (0x12/0x16/0xB0/0xB1)
Set_Display_On_Off(0x00); // Display Off (0x00/0x01)
Set_Display_Clock(0xF1); // Set Clock as 90 Frames/Sec
Set_Multiplex_Ratio(0x7F); // 1/128 Duty (0x0F~0x7F)
Set_Display_Offset(0x00); // Shift Mapping RAM Counter (0x00~0x7F)
Set_Start_Line(0x00); // Set Mapping RAM Display Start Line (0x00~0x7F)
Set_Remap_Format(0x74); // Set Horizontal Address Increment
// Column Address 0 Mapped to SEG0
Set_GPIO(0x00); // Set Low Voltage Level of SEG Pin
Set_Function_Selection(0x01); // Enable Internal VDD Regulator
// Select 8-bit Parallel Interface
Set_VSL(0xA0); // Enable External VSL
Set_Contrast_Color(0xC8,0x80,0xC8); // Set Contrast of Color A (Red)
// Set Contrast of Color B (Green)
// Set Contrast of Color C (Blue)
Set_Master_Current(Brightness); // Set Scale Factor of Segment Output Current Control
Set_Gray_Scale_Table(); // Set Pulse Width for Gray Scale Table
Set_Phase_Length(0x32); // Set Phase 1 as 5 Clocks & Phase 2 as 3 Clocks
Set_Precharge_Voltage(0x17); // Set Pre-Charge Voltage Level as 0.50*VCC
Set_Display_Enhancement(0xA4); // Enhance Display Performance
Set_Precharge_Period(0x01); // Set Second Pre-Charge Period as 1 Clock
Set_VCOMH(0x05); // Set Common Pins Deselect Voltage Level as 0.82*VCC
Set_Display_Mode(0x02); // Normal Display Mode (0x00/0x01/0x02/0x03)
Fill_RAM(0x00,0x00); // Clear Screen
Set_Display_On_Off(0x01); // Display On (0x00/0x01)
}