help wanted programming usart0 of atmega162

Hello, im having big big problems programming usart0 of atmega162. Below is the code of my program. im using stk500.

please could you tell me how can i make it works?

tell me also if its possible the configuration of fuse and lock bits to compare with the one i have.

when i turn on the microcontroller (programmed) conected to the hyperterminal i doesnt anything.

i want 9600bauds, no parity, 8 bits and 1 stop bit.

believe me im dont know what to do because with atmega16 it worked well.

i dont know what im doing wrong but i hope you do. Some part in the code are in spanish, my mother tongue.

thakns you very very much.

#include <avr/io.h>

// PROTOTIPOS DE FUNCIONES UTILIZADAS

void serial_init_0 (void);

unsigned char serial_recv_0 (void);

void serial_send_0 (unsigned char);

void serial_print_0 (const char *);

/* Inicia el puerto de la UART0 */

void serial_init_0(void) {

#define BAUD 3686000/16/9600-1

UBRR0L = 23;//ESTO SE SACA DEL DATASHEET

//ACTIVAR ENVIO Y RECEPCION

UCSR0B = (1<<TXEN0)|(1<<RXEN0);

//TIPO DE FRAME

UCSR0C = (1<<URSEL0)|(1<<USBS0)|(3<<UCSZ00);

return;

}

/* ESPERAR UN CARACTER Y DEVOLVERLO UART0*/

unsigned char serial_recv_0 (void) {

/* Esperar */

while (!(UCSR0A & (1 << RXC0)));

/* Devolver lo recibido*/

return UDR0;

}

/* ENVIAR UN CARACTER UART0*/

void serial_send_0 (unsigned char c) {

/* Esperar a que el buffer de envio esté vacio*/

while (!(UCSR0A & (1 << UDRE0)));

/* poner en UDR para enviarlo */

UDR0 = c;

return;

}

/* ENVIA UNA CADENA POR EL PUERTO SERIE UART0*/

void serial_print_0 (const char *msg) {

while (*msg != 0)

serial_send_0 (*msg++);

return;

}

int main() {

int i;

serial_print_0(“Hello”);

}

The first thing to check is the “clock divide by 8” fuse. If that is set, your clock is running at 1/8 the speed you think it’s running. I think it’s called CLKDIV or something similar. Also make sure the “output clock on pin PB0” (or whatever it is on your MCU) fuse isn’t set either. Also the #define BAUD in your setup routine isn’t being used for anything, but I assume that the value 23 is correct based on the table in the datasheet?