i am using an NTC thermistor and MSP430 to measure temperature between 0 to 50 degC.
ADC10 in msp is programmed to take 32 readings. the first 1-2 readings are quite away from the rest of readings. eventually the readings are stable with a couple of counts different.
Also when I power up the system first 4-5 sets of readings are quite away. they are literally off by 4-5degC, because the ADC readings are off.
has anybody faced same issue.
Also can some please commment on what is the best technique to average these readings.
Check the user guide for recommended capacitors and layout but it is typically a 10uF in parallel with a 0.1uF as close to the Vref pin as possible. I am using an MSP430F248 with the 12-bit ADC and the counts are VERY consistent. Of course, it depends upon the application and the layout. YMMV.