I am planning to create a remote controlled car with four 12v DC motors (four wheels). I have done a similar project on a much smaller scale using the L293D Duel H Bridge. However, this IC will not work for my new project because the current will be significantly higher. The 12v motors I plan to use have a max stall current of 10A each. I would like to drive 2 seperate channels in order to steer the car. I would like instant switching and the use of PWM. What options do I have to drive my remote controlled car when it comes to IC’s/driver boards?
Hi,
you can use Motor Driver 15A IRF7862PBF from sparkfun. site: https://www.sparkfun.com/products/9107