Hello,I have just bought the development board Apollo 3 Blue,serial basic breakout CH340C and the camera HM01B01. I have taken several photos based on the third example in Using SparkFun Edge Board with Ambiq Apollo3 SDK - SparkFun Learn, but I wonder:1. If I can take videos with it and set the shooting parameters for photos taken like resolution and size and so on.2.Or can anybody tell me what parameters am I able to set with the HM01B01, thanks a lot!
- 
You could certainly do so via a python script, but we don’t have a ready-made example…you just alter the photo example to iterate through X times with Y filenames
 - 
This probably won’t be very straightforward, but here’s the main src folder for the cam SparkFun_Apollo3_AmbiqSuite_BSPs/common/third_party/hm01b0 at 6398086a1a87ddea78274521683ba3ad817bee82 · sparkfun/SparkFun_Apollo3_AmbiqSuite_BSPs · GitHub, or just alter the parameters in a 2nd post-process python script (my inner lazy thinks this is what I’d do)
 
OK,thank you for your kind help!