How good is library support for Artemis features?

How available and stable are the Arduino IDE libraries for the Artemis features such as BLE Bluetooth?

I’m concerned that the Ambiq Apollo Blue 3 chip is a wonderfully functional chip…but…that the usual libraries to control the hardware aren’t there yet, or are not fully implemented, or are so unique that much of the application code has to be heavily modified to work.

There is a great benefit sometimes to using an older architecture that is more widely supported.

What’s the situation with the Artemis? How well supported it is and how much trailblazing is there?

Hi SeattleDavid,

The Apollo3 Arduino Core is still being actively developed but currently, BLE is not implemented in the [SparkFun Apollo3 Arduino Core. The page I linked is the best place to keep track of development status for our Arduino core for the Apollo3. [This issue also has an update from one of the engineers working on the Arduino core.](BLE support · Issue #22 · sparkfun/Arduino_Apollo3 · GitHub)](GitHub - sparkfun/Arduino_Apollo3: Arduino core to support the Apollo3 microcontroller from Ambiq Micro)