Hi,
i have a question. I have an arduino pro mini wired with an mpr121 and and openlog. everything works perfect. now i want to connect an rtc control.
I stick to this example code: http://wiring.org.co/learning/libraries … clock.html
SDA of rtclock is accordingly connected to digital pin 9, scl to digital pin 8, gnd to gnd or arduino and 5v to vcc in this case of openlog, as my arduino there was full, hope this doesnt matter.
this is the realclock code
#include <Wire.h>
int clockAddress = 0x68; // This is the I2C address
int command = 0; // This is the command char, in ascii form, sent from the serial port
long previousMillis = 0; // will store last time Temp was updated
byte second, minute, hour, dayOfWeek, dayOfMonth, month, year;
byte test;
// Convert normal decimal numbers to binary coded decimal
byte decToBcd(byte val)
{
return ( (val/10*16) + (val%10) );
}
// Convert binary coded decimal to normal decimal numbers
byte bcdToDec(byte val)
{
return ( (val/16*10) + (val%16) );
}
// 1) Sets the date and time on the ds1307
// 2) Starts the clock
// 3) Sets hour mode to 24 hour clock
// Assumes you're passing in valid numbers,
// Probably need to put in checks for valid numbers.
void setDateDs1307()
{
// Use of (byte) type casting and ascii math to achieve result.
second = (byte) ((Serial.read() - 48) * 10 + (Serial.read() - 48));
minute = (byte) ((Serial.read() - 48) *10 + (Serial.read() - 48));
hour = (byte) ((Serial.read() - 48) *10 + (Serial.read() - 48));
dayOfWeek = (byte) (Serial.read() - 48);
dayOfMonth = (byte) ((Serial.read() - 48) *10 + (Serial.read() - 48));
month = (byte) ((Serial.read() - 48) *10 + (Serial.read() - 48));
year= (byte) ((Serial.read() - 48) *10 + (Serial.read() - 48));
Wire.beginTransmission(clockAddress);
Wire.write(byte(0x00));
Wire.write(decToBcd(second)); // 0 to bit 7 starts the clock
Wire.write(decToBcd(minute));
Wire.write(decToBcd(hour)); // If you want 12 hour am/pm you need to set
// bit 6 (also need to change readDateDs1307)
Wire.write(decToBcd(dayOfWeek));
Wire.write(decToBcd(dayOfMonth));
Wire.write(decToBcd(month));
Wire.write(decToBcd(year));
Wire.endTransmission();
}
// Gets the date and time from the ds1307 and prints result
void getDateDs1307() {
// Reset the register pointer
Wire.beginTransmission(clockAddress);
Wire.write(byte(0x00));
Wire.endTransmission();
Wire.requestFrom(clockAddress, 7);
// A few of these need masks because certain bits are control bits
second = bcdToDec(Wire.read() & 0x7f);
minute = bcdToDec(Wire.read());
// Need to change this if 12 hour am/pm
hour = bcdToDec(Wire.read() & 0x3f);
dayOfWeek = bcdToDec(Wire.read());
dayOfMonth = bcdToDec(Wire.read());
month = bcdToDec(Wire.read());
year = bcdToDec(Wire.read());
Serial.print(hour, DEC);
Serial.print(":");
Serial.print(minute, DEC);
Serial.print(":");
Serial.print(second, DEC);
Serial.print(" ");
Serial.print(month, DEC);
Serial.print("/");
Serial.print(dayOfMonth, DEC);
Serial.print("/");
Serial.print(year, DEC);
}
void setup() {
Wire.begin();
Serial.begin(57600);
}
void loop() {
if (Serial.available()) { // Look for char in serial que and process if found
command = Serial.read();
if (command == 84) { //If command = "T" Set Date
setDateDs1307();
getDateDs1307();
Serial.println(" ");
}
else if (command == 81) { //If command = "Q" RTC1307 Memory Functions
delay(100);
if (Serial.available()) {
command = Serial.read();
// If command = "1" RTC1307 Initialize Memory - All Data will be set to 255 (0xff).
// Therefore 255 or 0 will be an invalid value.
if (command == 49) {
// 255 will be the init value and 0 will be cosidered an error that
// occurs when the RTC is in Battery mode.
Wire.beginTransmission(clockAddress);
// Set the register pointer to be just past the date/time registers.
Wire.write(byte(0x08));
for (int i = 1; i <= 27; i++) {
Wire.write(byte(0xff));
delay(100);
}
Wire.endTransmission();
getDateDs1307();
Serial.println(": RTC1307 Initialized Memory");
}
else if (command == 50) { //If command = "2" RTC1307 Memory Dump
getDateDs1307();
Serial.println(": RTC 1307 Dump Begin");
Wire.beginTransmission(clockAddress);
Wire.write(byte(0x00));
Wire.endTransmission();
Wire.requestFrom(clockAddress, 64);
for (int i = 1; i <= 64; i++) {
test = Wire.read();
Serial.print(i);
Serial.print(":");
Serial.println(test, DEC);
}
Serial.println(" RTC1307 Dump end");
}
}
}
Serial.print("Command: ");
Serial.println(command); // Echo command CHAR in ascii that was sent
}
command = 0; // reset command
delay(100);
}
When i try to upload the code as a new file nothing moves, then even my mpr121 doesnt work. so do i have to insert this code in my mpr121 code or how does it go to go with the rtc?
tks