iso9
1
Hi,
I’m new with the MSP430, and i just downloaded the MSPGCC compiler but i’m not too sure how i’m suppose to compile files?
ie. what does the makefile do
also i downloaded the TCPIP example from http://www.mikrocontroller.net/mspgcc.en.htm
and i’m trying to compile it.
Any step by step examples would be helpful!!!
OLIMEX
2
using GCC tools is not very convenient for Windows users, once you config the compiler and environment it’s pretty easy though.
microcontroller.net have a lot of info, just read and follow the instructions
I never happend to run it on Windows/Cygwin as the debugger chrashes constantly on the Win98 I tried
Tsvetan
system
3
Thanks for the reply,
I’ve been reading and i’m still a little confused on how i’m suppose to compile it.
Like when i download the files, it contains a makeful.
what does this file do? Also the set of code i downloaded has a readme.txt and i’m not sure what all the flags do.
here’s what it says to compile the file
msp430-gcc -O easyweb.c -mmcu=msp430x149 -o tcpip -Wall
what does the -wall do?
Plus i get a lot of errors when i try this
i get errors like this:
undefined reference to ‘TxFrame1’
/cygdrive/c/DOCUME~1/user/LOCALS~1/Temp/ccapk7GB.o<.text+0x6b8>: In function ‘HTTPServer’:
i have nooo idea what this means =)
Any help would be appricated.
Thanks
iso9
4
Ok i figured out my problems… =)