How to install one thermostat?Is there anyone use it ?

How to install one thermostat(temperature controller)?Is there anyone use it for home brew .The device information like following:

Detailed Product Description

Measure range:-50~+99°C

Mounting size:71*29mm

Auto switch between refrigerating and heating

Retrun difference value

All-purpose Temperature Controller STC-1000:

Features:

Switch the modes between cool and heat; Control temperature by setting the temperature setting value and the difference value; Temperature calibration; Refrigerating control output delay protection; Alarm when temperature exceeds temperature limit or when sensor error.

Specification and Size:

1.Front panel size75(L)×34.5(W)mm;

2.Mounting size:71(L)×29(W)mm;

3.Product size75(L)×34.5(W)×85(D)mm;

4.sensor length2minclude the probe.

Technical Parameters:

  1. Temperature measuring range: -50~99oC;

  2. Resolution: 0.1°C; 3. Accuracy: ±1°C (-50~70°C);

  3. Sensor error delay: 1 minute

  4. Power supply: 110VAC±10%, 50/60Hz;

  5. Power consumption: ≤3W;

  6. Sensor: NTC sensor (1PC);

  7. Relay contact capacity: Cool 10A/250VAC;Heat 10A/250VAC;

  8. Ambient temperature: 0~60°C;

10.Storage temperature: -30~75°C;

11.Relative humidity: 20%~85% (No condensate).

What do you mean install it? Do you mean how to connect it to a controller?

codlink:
What do you mean install it? Do you mean how to connect it to a controller?

Oh ,yes ,I don;t know how to connect it.

Look at the side of the STC-1000; the picture describes the connections. Also, do a google search for “STC-1000”. There are many hits. This one http://brewprof.com/weekend-diy-homebre … -stc-1000/ shows how to mount the controller in a box with two controlled outlets on the output.

This thread http://www.homebrewtalk.com/showthread.php?t=330427 goes into details on how to add relays to power larger loads.

/mike

n1ist:
Look at the side of the STC-1000; the picture describes the connections. Also, do a google search for “STC-1000”. There are many hits. This one http://brewprof.com/weekend-diy-homebre … -stc-1000/ shows how to mount the controller in a box with two controlled outlets on the output.

This thread http://www.homebrewtalk.com/showthread.php?t=330427 goes into details on how to add relays to power larger loads.

/mike

:clap: :clap: :clap:

Thank you so much !

This videos tell us how to connect one PID temp. controller but I’d like to know how to connect one ITC-1000F

https://youtu.be/DZDkrR0Vhrc

The manual tells all:

http://www.ink-bird.com/asset/file/ITC-1000F_EN.pdf

DanV:
The manual tells all:

http://www.ink-bird.com/asset/file/ITC-1000F_EN.pdf

Thank you.