I have a Micromod Single Main Board. When I plug an I2C device into the qwiic connector that is horizontal / on the edge of the board, all works fine.
However, when I plug the same device into the connector that is vertical / perpendicular to the main board I am unable to see the device.
Do both connectors share the same Wire? Or is there a change in code required to use the 2nd qwiic connector?
Thanks,
Mike
Both connect to the same thing on the main board and don’t require any changes to your code.
Does your sensor work if you plug into the not working connector then disconnect and reconnect power?
(or reset your sketch) Some Qwiic devices don’t behave properly if you unplug and replug them with power on and sketch running.
Only the one connector is working. The other (which is the one I need for mounting reasons) appears to be INOP. Even after rebooting/reloading everything.
Sounds like you have a board with a bad socket.