hello.
I’d like to ask you questions while using RTK after watching “RTK Express Hookup Guide”.
- What does “Mean” mean in the survey procedure at Base Station?
As a result of the test, if 30 satellites are used and move on to the survey procedure, “Mean” will be lowered to 0.7. (If “Time” is set to 600 seconds via S/W)
- We are communicating base and rover through 915 MHz communication, but why is it because it is disconnected in the following cases?
-. Base setting: “configuration base → Set required Mean 3D standard development : 1 meter”
-. Rover Settings: Configuration Base → Set required Mean 3D Standard Deviation : 5 meters"
When I set Base and Rover to “5 meters” because I couldn’t communicate, it became 915Mhz communication. I wonder if it’s because it’s programmed on S/W or if it’s an error.
(Tested in a place without radio interference.)
…