Hi, I am researching making a small multi-band GPS device and the Postcard+Port. Shield, etc, seem to make it as easy as it’s going to get. I am concerned about how water-tight the enclosure is. I’m not expecting to reach IP67, but I don’t want to have to worry about it. I’m used to using a garmin glo, with just a few indicator led’s.
I’m wondering if I could achieve that if I left out the shield and put the board in a clear waterproof enclosure with holes for just the USB and antenna (and something for boot/reset/power). It seems that I’d at least have to add back a charger in this configuration. Would I be able to achieve my goals using the 290P-only breakout and the ESP32-C6 Pocket Dev Board ? Can that board run the RTK Everywhere firmware?
Thanks,
Greg